Unable to boot from Satellite C55-A

Reply
Member
Posts: 3

Unable to boot from Satellite C55-A

[ Edited ]

Hi, everyone

 

I messed up my system and now I can not boot into Win8, when I hit the power button, I can only see toshiba's logo and a loading bar under it, and the loading bar keeps loading forever but nothing happens.

 

I tried to fix it as bootloader problem, by following this article: http://superuser.com/questions/460762/how-can-i-repair-the-windows-8-efi-bootloader

 

But no magic happens, it's just keep loading on start. And One Interesting thing is, after I re-enter into recovery command line, and go to EFI\Microsoft\Boot, I found the BCD file that I created before was removed!!

 

And I tried commands in command line of the recovery gui, following this article: http://www.techspot.com/guides/630-windows-8-boot-fix/

And when I reach to this command:  bootrec /rebuildbcd

 

I will get the following message:

The requested system device cannot be identified due to multiple indistinguishable devises potentially matching the identification criteria

 

Can anyone please help me. I don't actually know what should I do.

 

Also, in the EFI partiion I found two efi boot folder, one is microsoft, one is toshiba. I don't know if toshiba has it's own settings, and should I recover my system based on that?

 

Thanks

Frequent Advisor
Posts: 2,331

Re: Unable to boot from Satellite C55-A

[ Edited ]

Hi! I have no life so I hang out here on the forum on week ends. Most of the other advisors have a life! Please post your full model number found on the bottom of your lap top. I do not run W8. You will get better replies during the week. My advice is to save your data and restore to factory settings.

http://forums.toshiba.com/t5/Windows-8-Knowledge-Base/What-can-I-do-if-my-Windows-8-laptop-won-t-sta...

System recovery discs and USB recovery can be found here. I recommend the USB.

Dokie!!

I Love my Satellite L775D-S7222 Laptop. Some days you're the windshield, Some days you're the bug. The Computer world is crazy. If you have answers to computer problems, pass them forward.
Member
Posts: 3

Re: Unable to boot from Satellite C55-A

[ Edited ]

Thanks for your reply!

 

My model is C55-A5286

 

I just got it 4 days ago.

 

 

One thing I found that's interesting is, when I went to command line, and use diskpart to list vol, I found my windows partition is hidden!! I don't know how the hell it became hidden. I think that might be the reason that even repair bcd is failed.

Frequent Advisor
Posts: 2,331

Re: Unable to boot from Satellite C55-A

Hi ! Your model is so new that Product Support doesn't show specs or user guild. I know very little about W8??

I would take it back to the sellerSmiley Wink

Dokie!!

I Love my Satellite L775D-S7222 Laptop. Some days you're the windshield, Some days you're the bug. The Computer world is crazy. If you have answers to computer problems, pass them forward.
Frequent Advisor
Posts: 2,331

Re: Unable to boot from Satellite C55-A

Hi ! This is the best I can do for you. There should be more replies during the week.Smiley Wink

http://forums.toshiba.com/t5/Windows-8-Knowledge-Base/What-can-I-do-if-my-Windows-8-laptop-won-t-sta...

I Love my Satellite L775D-S7222 Laptop. Some days you're the windshield, Some days you're the bug. The Computer world is crazy. If you have answers to computer problems, pass them forward.
Member
Posts: 3

Re: Unable to boot from Satellite C55-A

Hi, Dokie

 

Thanks for your reply. I've tried these methods but none of them is working.

 

But yeah, I finnally gave up and went to store for an exchange. 

 

Again thank you very much for your help. Looks like we all have no life. Smiley LOL

Frequent Advisor
Posts: 2,331

Re: Unable to boot from Satellite C55-A

Hi! Thanks for your reply!

Dokie!Smiley Wink

I Love my Satellite L775D-S7222 Laptop. Some days you're the windshield, Some days you're the bug. The Computer world is crazy. If you have answers to computer problems, pass them forward.
Posts: 47,926
Topics: 85
Kudos: 9,130
Solutions: 3,230
Registered: ‎12-04-2008

Re: Unable to boot from Satellite C55-A


Your model is so new that Product Support doesn't show specs or user guild.


The Manuals and Specs tab appears to be broken for the weekend. But you can usually hunt down the spec for new machines.

 

   Satellite C55-A5286

-Jerry
Channel 9