04-29-2011 03:23 PM - edited 04-29-2011 03:23 PM
I recently recovered from malware, and would really like to recover the netbook to out-of-box state. I've found the links to order the recovery USB (this netbook does not have a DVD drive). The manual suggests creating/using recovery media on either DVD or USB.
In checking out the boot menu though, it doesn't appear to have a "Boot From USB" option. It only shows HDD/FDD or LAN.
The only thing I can think of is, when a bootable USB is attached (at start-up), the boot menu will recognize it, however, my experience with BIOS/boot menus, this isn't expected behavior (it should show up as an option whether or not something is connected).
Is there any way to do recovery of this netbook?
Refers to: Toshiba NB505-N500BL Netbook with Win7 Starter Pre-Installed
Solved! Go to Solution.
04-29-2011 03:37 PM
The only thing I can think of is, when a bootable USB is attached (at start-up), the boot menu will recognize it..
I think you'll find that when there is a drive plugged in, the BIOS does indeed show USB in the boot sequence.
Notice in the section Restoring from recovery DVDs/media, which begins on p. 60, you are instructed to insert the USB flash drive before turning on the computer.
04-29-2011 03:51 PM
Bang! Yes, there it is. It's funny how I thought I "tried everything". Everything but the one thing that I didn't expect to work. Thanks for the quick response!
04-29-2011 04:12 PM
You're welcome. Happy to help.
09-01-2011 05:00 AM
sir, good day, can i have a copy of this recovery software for NB505?
I cannot format my new NB505-N500BL to a new Windows 7 Starter OS.
Thanks for your advance help.
07-10-2012 01:52 PM
Hello, do you have the link where we can order the recovery USB for the NB505-N500BL? (A clean install of Windows was done on mine & I can't access the recovery partition.)
07-10-2012 02:21 PM
09-13-2012 02:31 AM
Hi,
I bought my NB505-N500BL in USA, but I am living now in Bulgaria.
Do you know how can I order USB recovery, when my country is not in the ''country'' list and the form is not accepting my actual address?
09-13-2012 08:45 AM
I am living now in Bulgaria.
So far as I know, you will need to make arrangements with an acquaintance in a country Toshiba America ships to and have it reshipped.
09-13-2012 10:11 PM
Thank you Jerry!
09-14-2012 05:42 AM
Good luck!
Copyright © 2013 Toshiba America Information Systems, Inc. All rights reserved.