06-19-2010 08:50 PM
Hi, I've had my Satellite for almost two years but need to restore all my factory settings. I've tried everything, from holding down "0" or "C" but nothing seems to work. I don't have the disks and I'm really at a loss, since I use my laptop for mainly schoolwork. Any helpful suggestions would be greatly appreciated ![]()
Solved! Go to Solution.
06-20-2010 08:16 PM
Help, anyone? :]
06-21-2010 02:04 PM
See the section Hard Drive Recovery Utilities, which begins on p. 60 of the User's Guide.
Satellite M300 Series User’s Guide
You can discover which recovery features you have this way.
If you cannot restore directly from a recovery partition, then burn the recovery discs.
If you cannot burn the recovery discs, then order them from Toshiba.
06-24-2010 02:16 PM
Thank you, that helped :]
06-24-2010 02:43 PM
Good.
Copyright © 2013 Toshiba America Information Systems, Inc. All rights reserved.