02-03-2011 05:48 PM
I have the above mentioned computer and it is 2 years old. Last year in January the hard drive crashed and had to have new one installed at Best Buy. Now it will not start up. When I turn it on the Toshiba screen displays with F2 and F12 options. Then the creen goes black and the following displays:
Intel UNDI, PXE-2.1 (build 082)
Copyright (C) 1997-2000 Intel Corporation
For realtek RTL8101E/8102E PCI-E Ethernet Controller v1.07 (080320)
PXE-E61: <edia test failure, check cable
PXE-MOF: Exiting PXE ROM
No bootable device -- insert boot disk and press any key
I insert the recovery CD and it says windows loading files then has a screen that says Selecting a Process: Toshiba Recovery Wizard or System Recovery Options. I choose System Recover Options and then choose English language and US keyboard layout. Then the following screen comes up: Select an operating system to repair .... If you do not see your operating system listed click Load Drivers to load drivers for your hard disks. When I choose Load Drivers I do not know where to find the OS driver. When I click Next and choose Startup Repair it says it is unable to fix the problem automatically.
I don't want to choose Toshiba recover Wizard because it says it will erase everything. Does anyone have any suggestions on how to fix this problem?
02-06-2011 08:06 AM
The exact same thing happened to me yesterday Feb 5!!!
During normal use of windows 7 the computer crashed and went through the same boot procedure as described by the previous poster.
Now I can't do anything with my hard drive. I tired everything. I even tried restoring it from the backup image that I have, but it said that it cannot find hard drive!
I do not have Toshiba Recovery. Can I download it from somewhere?
Does anyone have any suggestions? After booting from Win 7 Recovery Disk, I even tried fixing the MBR and partitions, but I would always get an error message that the system doesn't support the software I tried using (guessing because it's 64bit?)
Please, any suggestion is most welcome and appreciated!!!
Thanks,
Djape
02-09-2011 12:02 PM
Hello jrpetty45. You wrote : I don't want to choose Toshiba recover Wizard because it says it will erase everything.
You also wrote that this is a new HD ! What is there to loose ? Get back to me on this, nobody else has tried to help you but it must be possible to do something. Do you have a bootable disk of any kind ? Did you make the Recovery DVDs as instructed when you first got the laptop ? They are bootable, insert the #1, shut down the machine and restart, it should seek the DVD and boot.
Did you replace the HD yourself and what is an honest level of knowledge here ? So many questions but help us help you. JP.
02-16-2011 07:32 AM
Copyright © 2013 Toshiba America Information Systems, Inc. All rights reserved.