Toshiba Satellite A135-S7404 Laptop start up issue

Reply
Member
Posts: 2

Toshiba Satellite A135-S7404 Laptop start up issue

[ Edited ]
 

Intel UNDI, PXE-2.1 (build 082)

Copyright (C) 1997-2000 Intel Coporation 

 

 

For Realtek RTL8100E/8101E Fast Ethernet Network Adapter v1.02 (060510)

PXE-E61: Media Test Failure, Check cable

PXE-MOF: Exiting PXE ROM.

 

 

Frequent Advisor
Posts: 2,331

Re: Toshiba Satellite A135-S7404 Laptop start up issue

Hi ! Try here!

Dokie!!

I Love my Satellite L775D-S7222 Laptop. Some days you're the windshield, Some days you're the bug. The Computer world is crazy. If you have answers to computer problems, pass them forward.
Regular Advisor
Posts: 1,345

Re: Toshiba Satellite A135-S7404 Laptop start up issue


quickfoot wrote:
 

Intel UNDI, PXE-2.1 (build 082)

Copyright (C) 1997-2000 Intel Coporation 

 

 

For Realtek RTL8100E/8101E Fast Ethernet Network Adapter v1.02 (060510)

PXE-E61: Media Test Failure, Check cable

PXE-MOF: Exiting PXE ROM.

 

 


could be a problem within your OS system files or may be a hardware issue causing the dreaded boot loop.  Do you have a set of recovery disks?  If not, you likely need to order them from Toshiba and see if you can do a Repair Operating System.  If that doesn't work you can use the recovery disks to return the computer back to "out-of-box" state but will loose all of your personal data.  You may be able to retreive personal data if the drive can be read using another computer. 

L305-S5955, T9300 Intel Core 2 Duo, 4GB RAM, 120GB SSD, Win 7 Ultimate 64-bit