Satellite L650

Reply
Member
Posts: 2

Satellite L650

I would like to restore my satellite L650 to factory settings. Do I need to purchase the quick restore cd to do this? Or can it be done by holding down the zero key? I have already backed up and removed data music & photos.
Thanks
Penelope
Posts: 46,771
Topics: 83
Kudos: 8,791
Solutions: 3,145
Registered: ‎12-04-2008

Re: Satellite L650

Always tell us which Satellite L650 you have. See the label on the bottom. Procedures can be somewhat different depending on the part-number family.

 

If this is a US computer, see the section Recovering the Internal Storage Drive, which begins on p. 59 of the User's Guide.

 

   Satellite L640/L650 Series User’s Guide

-Jerry
Channel 9
Member
Posts: 2

Re: Satellite L650

Hello Jerry,

 

reading the bottom, model number PSK1JA-OK5017 or is there another number to look for?

hope this helps. I am in Australia.

thanks

Posts: 46,771
Topics: 83
Kudos: 8,791
Solutions: 3,145
Registered: ‎12-04-2008

Re: Satellite L650

 

Satellite L650/0K5 (PSK1JA-0K5017)

 

Your downloads are here, Penelope.

 

You can indeed restore the hard disk to its original out-of-the-box contents using Toshiba recovery media. And you can do it directly from a partition on the hard drive. See the section System Recovery, which begins on p. 1-13 of your (very extensive) User's Manual.

 

I recommend that you first create recovery disks from that partition in case something goes wrong.

 

   Users Manual 1.0 for Windows 7 32-bit (40 MB)

   userguidel650.pdf

-Jerry
Channel 9