Reply
Member
Posts: 2

Satellite L355-S7907 Recovery Error 10-FC12-045D

[ Edited ]

Laptop would not boot  into Windows (Vista)(a *.sys file missing)

Toshiba Recovery Wizard after an hour Error 10-FC12-045D (4 attempts)

Toshiba tool FJDT_V690 cannot find the drive, suggests it is disconnected, but running this from a DOS Boot CD.

Another DOS based diag shows countless bad sectors and "Read Element" error.

Would like to find a DOS utility which would unhide the recovery partition then allow to create an Image file to DVD.  Problem is it cannot be a utility which must install on the hard drive.

 

Ghost and Drive Image do not see this hidden partition (I believe it is Drive F:smileyhappy:

Have new drive, but don't want to wait for Tosh to send a Recovery Disk

If can't copy the recovery partition to install Vista on new drive then plan to install XP Pro.  I found the Toshiba Drivers for Win XP sp2/sp3. 

Will this Laptop/components work with XP Pro?

 

Thx

Regular Contributor
Posts: 118

Re: Satellite L355-S7907 Recovery Error 10-FC12-045D

http://www.csd.toshiba.com/cgi-bin/tais/support/jsp/bulletin.jsp?soid=2115348

 

"An error has occurred. ERROR :10-FC10-1710" -- may be caused by a faulty hard drive.

"An error has occurred. ERROR :10-FC12-0241" -- may be caused by a faulty hard drive or defective memory.

"An error has occurred. ERROR :10-FC12-045D" -- may be caused by a faulty hard drive.

"An error has occurred. ERROR :10-FC06-0002" -- may be caused by damaged recovery media or faulty hard drive.

"An error has occurred. ERROR :10-FC12-0970" -- may be caused by defective memory.

Member
Posts: 2

Re: Satellite L355-S7907 Recovery Error 10-FC12-045D

Apparently the above link is only viewable to Toshiba Partners as it requires login.  Could it be posted here?