Restoring Qosmio f60-00m to factory settings WITHOUT cd?

Reply
Member
Posts: 1
Accepted Solution

Restoring Qosmio f60-00m to factory settings WITHOUT cd?

I believe my parents threw out the box my laptop came in with all the recovery CDs and what not. Is there any way to restore my laptop to its factory settings without any type of CD?

 

Thanks in Advance.


Accepted Solutions
Posts: 47,103
Topics: 83
Kudos: 8,931
Solutions: 3,171
Registered: ‎12-04-2008

Re: Restoring Qosmio f60-00m to factory settings WITHOUT cd?

 

Qosmio F60-00M (PQF65C-00M02D)

 

See the section Restoring the pre-installed software from the Recovery hard disk drive, which begins on p. 1-14 of the User's Manual (attached).

 

I've also attached the specs for that model.

-Jerry
Channel 9

View solution in original post


All Replies
Posts: 47,103
Topics: 83
Kudos: 8,931
Solutions: 3,171
Registered: ‎12-04-2008

Re: Restoring Qosmio f60-00m to factory settings WITHOUT cd?

 

Qosmio F60-00M (PQF65C-00M02D)

 

See the section Restoring the pre-installed software from the Recovery hard disk drive, which begins on p. 1-14 of the User's Manual (attached).

 

I've also attached the specs for that model.

-Jerry
Channel 9