Reformat and Recovery of Satellite L775

Reply
Member
Posts: 2
Accepted Solution

Reformat and Recovery of Satellite L775

[ Edited ]

On Windows XP I cleaned up my system periodically by reformatting and re-installing the OS. I have a Toshiba Satellite  L775, running Windows 7 Home Premium, 64 bit.  I have the recovery media that I made when I started using the computer (though it seemed like many disks for this).  I have not reformatted the disk yet, so I have the disk image too (apparently).  I have a current backup of all my programs and files.  Is it a bad idea to continue this cleanup procedure (reformat and reinstall) that I have used for several years?

 

Paul

Posts: 4,810
Topics: 56
Kudos: 1,535
Solutions: 370
Registered: ‎05-03-2009

Re: Reformat and Recovery of Satellite L775

[ Edited ]

I think it's a good idea, Paul.  And you can use the disks you made or use the recovery partition which is on the HDD by holding down Zero while turning the computer on.  Doesn't take very long and you get to start all over again with the equivalent of a new machine. See the section in your User's Guide "Recovery of internal storage drive". You don't have to "reformat" any more; that's taken care of automatically.

 

C.B.

C.B.

Toshiba Sat. C75D-B7260 Win 8.1 64 Bit--Toshiba Sat. L775D-S7132 Win 7 HP SP1 64 Bit and Win 10 PRO Insider Preview--Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit--Toshiba Sat. Radius P25W-C2300-4K Win 10 Home 64 Bit

View solution in original post


All Replies
Posts: 4,810
Topics: 56
Kudos: 1,535
Solutions: 370
Registered: ‎05-03-2009

Re: Reformat and Recovery of Satellite L775

[ Edited ]

I think it's a good idea, Paul.  And you can use the disks you made or use the recovery partition which is on the HDD by holding down Zero while turning the computer on.  Doesn't take very long and you get to start all over again with the equivalent of a new machine. See the section in your User's Guide "Recovery of internal storage drive". You don't have to "reformat" any more; that's taken care of automatically.

 

C.B.

C.B.

Toshiba Sat. C75D-B7260 Win 8.1 64 Bit--Toshiba Sat. L775D-S7132 Win 7 HP SP1 64 Bit and Win 10 PRO Insider Preview--Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit--Toshiba Sat. Radius P25W-C2300-4K Win 10 Home 64 Bit
Member
Posts: 2

Re: Reformat and Recovery of Satellite L775

Thank you very much.  Now all I need to do is do it.

 

Paul