L505 S5971 will not reboot

Reply
Member
Posts: 1

L505 S5971 will not reboot

At first, the webcam went out and then it was the sound and usb. That was two weeks ago, then this week it went as far as the TOSHIBA screen with the f2 and f12 screen. What do I do next to see if the HDD did not go out or is it some other problem? Your advice or help would be appreciate it. The laptop is almost 3 years old.

Posts: 21,718
Topics: 70
Kudos: 839
Solutions: 482
Registered: ‎10-04-2011

Re: L505 S5971 will not reboot

It won't boot now? What's the last thing displayed on the screen?

 

It should prompt you to press a key to view the boot menu. What happens when you press that? If the menu appears, what does it list?

- Peter