How to Create recovery disc

Reply
Member
Posts: 1

How to Create recovery disc

Hi I have installed windows 7 on my laptop it is satellite l500-12Q part number : PSLJ0E-00J009AR and after that all my function key is not working only the brightness one is working but the wifi and the touch pad is not so I need to install the original hdd recovery but when I tried shutting down the computer and pressing either zero (0) or F8 or F12 it don't want to boot so I need to make a recovery disc which I don't know how to do it I need the Toshiba recovery disc creator program to do it any help plzz?

 

Posts: 47,686
Topics: 85
Kudos: 9,090
Solutions: 3,214
Registered: ‎12-04-2008

Re: How to Create recovery disc


satellite l500-12Q (PSLJ0E-00J009AR)


Satellite L500-12Q (PSLJ0E-00J00NG3)  <--the EMEA version

 


I need to make a recovery disc which I don't know how to do


See the section Creating Optical Recovery Discs, which begins on p. 3-11 of the User's Manual (attached).

-Jerry
Channel 9