How do I install the operating system Windows 7 on a new hard drive?

Reply
Member
Posts: 1

How do I install the operating system Windows 7 on a new hard drive?

Good morning ¿ how I can install windows 7 home premium on a new hard drive?, Disk damage has my laptop windows 7 home premium 32 bit and I have to buy a new hard drive, but not as I have already installed the new because I do not have installation CD because it is laptop, thanks. My laptop is a satellite L455-S5975 .

 

For I CAN NOT get the recovery disks, and I'm not in USA. There will be a way to get it via download?

 

My English is not very good, excuse me if I do not understand.

Posts: 47,997
Topics: 85
Kudos: 9,136
Solutions: 3,233
Registered: ‎12-04-2008

Re: How do I install the operating system Windows 7 on a new hard drive?

 

Satellite L455-S5975 

 


I CAN NOT get the recovery disks, and I'm not in USA. There will be a way to get it via download?

There is no opportunity to download it, Richo. Your best bet is to have an acquaintance in the USA, Latin America, or Canada order the recovery discs and ship them to you.

-Jerry
Channel 9