Error Code 0A-0543-0000 When trying to Restore back to factory state

Reply
Member
Posts: 1

Error Code 0A-0543-0000 When trying to Restore back to factory state

Hello,

 

I keep getting Error code 0A-0543-0000 when trying to restore a Satellite L755 to the factory state either from the restore partition on the hard drive or when I use a restore cd.  The laptop was functioning ok before this operation.  Windows 7 was having some issue's, but would load and not crash.  Not sure if the hard drive is bad or?  Any help is greatly appreciated.

 

Thanks

 

C

Posts: 2,948
Topics: 35
Kudos: 2,113
Solutions: 163
Registered: ‎07-26-2013

Re: Error Code 0A-0543-0000 When trying to Restore back to factory state

[ Edited ]

You can try tapping f8 at start up and select repair your computer. 

S70-ABT2N22 Windows 7 & 8.1Pro, C55-A5180 Windows 8.1 & W 10 ****Click on White “Kudos” STAR to say thanks!****