Reply
Member
Posts: 3

Can't restore my A665-S6070 to factory settings

I'm having major problems with a Toshiba satellite A665-S6070 laptop I just got. It  won't boot up because of some error in the registry.  I have tried the restore to factory settings. After almost completing the restore it goes to checking the system performance and just shuts completely down. I can't get past this problem. What should I do? 

 

One other thing I'm not sure of.  I can't run my laptop from the charger unless the battery is removed.  Is that normal or do I have another problem?

 

Thanks for any help.

Frequent Advisor
Posts: 2,331

Re: Can't restore my A665-S6070 to factory settings

"I can't run my laptop from the charger unless the battery is removed.  Is that normal or do I have another problem?"

 No this is not normal and I suppose it could be causing problems restoring back to factory??

Send it back!!

Dokie!

I Love my Satellite L775D-S7222 Laptop. Some days you're the windshield, Some days you're the bug. The Computer world is crazy. If you have answers to computer problems, pass them forward.