01-22-2012 09:49 AM
Hello Sir.
I have a Toshiba Satellite L630-107.
The problem is that when I tried to restore to factory default, this message popped up "BOOTMGR is missing! Press Ctrl+Alt+del to restart" Please Help me as to how I could go through this. My laptop won't can't go back to its normal process without solving this issues.
What should I do? I admit I am not really good on how this things work. Where should I get this BOOTMGR. omg
Thank you so much.
-Anton
Solved! Go to Solution.
01-22-2012 09:58 AM
And everytime I press cntl Alt Del, it restarts and then goes back to" BOOTMGR is missing! Press Ctrl+Alt+del to restart". It seems I can't proceed to the next step without solving this even if I restart my Laptop.
Please help Sir.
Thank you.
-Anton
01-22-2012 12:27 PM
Satellite L630-107 (PSK04E-00P00QAR)
..when I tried to restore to factory default, this message popped up "BOOTMGR is missing! Press Ctrl+Alt+del to restart"
Anton, are you trying to recover using the image on the hard drive? If so, follow the instructions in the section Restoring the pre-installed software from the Recovery hard disk drive, which is at the top of p. 1-14 of your User's Manual (attached).
If that doesn't work, then burn the recovery discs using instructions in the section Creating Recovery Media at the top of p. 1-12. After that, restore the drive according to the section Restoring the pre-installed software from your created Recovery Media, which begins near the bottom of p. 1-14.
01-24-2012 12:33 AM
Thank you so much Sir Jerry.
-Anton
01-24-2012 06:57 AM
You're quite welcome. Happy to help out.
03-04-2012 10:59 AM
I got a new hard drive and when i placed it in there i turned on my computer and it came up "BootMgr" is missing
Press Ctrl+Alt+Del
Someone please help me solve this problem.
07-08-2012 06:26 AM
hi
I have the same problem but my case is something different. I have no os running or want to do recovery. I just want to install the win 7 Os to my laptop which has no os or empty. But whenever iam trying to bootup from my pendrive or cd i have the problem " BOOTMGR is missing".
Can u please suggest me regarding this.
Thanks
sunny.
09-19-2012 08:57 AM
hii sir,
i have Toshiba Satellite L750-X5318
My laptop was working properly till yesterday night
but when i pressed power button first thing appeared in screen is...
n nothing is working..
f8 f2 f6 nothing is taking me to anywhere... just beep sound comes whenevr i press a key except ctrl+alt+del
Please help me.... Tomorrow is my website launch.. n mine everything is in my laptop.....
Please.............
01-20-2013 01:55 PM
It is in a loop ( boot mgr missing to press control alt del ) this goes to press F2 or f12 takes me back to boot mgr missing. I have Toshiba Satellit L305D S5873 ) pressing anything dont help. Now what do I do. ???
does buying windows 7 or 8 help to fix the problem. I would like to save Documents and Pictures.
Is there anything i can buy or should i throw laptop away.??
Thanks
01-20-2013 01:58 PM
Eckhart1938 wrote:...
Start a new thread with your problem.
Copyright © 2013 Toshiba America Information Systems, Inc. All rights reserved.