Re: A505S6980 WON'T BOOT

Reply
Member
Posts: 1

A505S6980 WON'T BOOT

Was running malware and screen went to black with blinking cursur

Will not boot to windows 7. At F12 ,system repair disk brings up Toshiba recovery wizard and system recovery options. The recovery disk i made do not work and when i go to recovery options nothing works for me here.

System restore gives me an error message 0x8000ffff.

I'm at the reformatt the hard drive point but can't find a ay to do this.

F8 does not work, #0 at startup doesn't work.

Help

 

Highlighted
Posts: 48,235
Kudos: 9,199
Solutions: 3,265
Registered: ‎12-04-2008

Re: A505S6980 WON'T BOOT

 

Satellite A505-S6980

 


system repair disk brings up .. system recovery options


This?

 

   

-Jerry
Channel 9