Reply
Regular Advisor
billkunert
Posts: 268
0

13.55 gig unlettered primary partition after recovery

I just installed a 240 gig SSD in my computer and used my USB recovery thumb drive to load software and selected to set it the way it was when new.  I understand the 1.46gig recovery partition but I don't understand why it also creates a 13.55 gig primary partition with no drive letter.  Seems like wasted space and it did the same thing on the original 640 gig drive.  Go to the Start search window and type diskmgmt.msc to check your C drive.

L875D-S7232
Super Advisor
cbwilsha
Posts: 2,578
0

Re: 13.55 gig unlettered primary partition after recovery

How do you think an HDD or new HDD gets recovered to out-of-box with all the software it came with?  The 1.46GB partition is just the recovery operation software.  The 13.55GB partition is all of the original software installation. 

 

C.B.

C.B.
Toshiba Sat. L675D-S7016 Win 8 PRO 64 Bit---Toshiba Sat. L775D-S7132 Win 7 PRO SP3 64 Bit which also has Virtual Machine with Win XP SP3---Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit
Regular Advisor
billkunert
Posts: 268
0

Re: 13.55 gig unlettered primary partition after recovery

I guess that means I can eliminate that partition should I need more space since I started with a blank drive and a 16gig USB thumb drive.  It apparently doesn't serve a function unless you recover from the drive itself.

L875D-S7232
Ace Advisor
Jerry_Lippey
Posts: 33,108
0

Re: 13.55 gig unlettered primary partition after recovery

 

Satellite L875D-S7232

 


It apparently doesn't serve a function unless you recover from the drive itself.


Yes, it's used for recovering directly from the HDD to the original out-of-the-box contents and also to create recovery media.

 

I routinely remove that partition from computers with preinstalled OEM Windows.

 

If the 1.46 GB partition as labeled Active in Disk Management (diskmgmt.msc), then it contains the boot files as well as the recovery environment.

-Jerry