Which Ports are USB 3.0 Compatible

Reply
Member
Posts: 5
Accepted Solution

Which Ports are USB 3.0 Compatible

Does anyone know which ports on my NEW Satellite IPPP are USB 3.0 computable?

Posts: 46,770
Topics: 83
Kudos: 8,791
Solutions: 3,145
Registered: ‎12-04-2008

Re: Which Ports are USB 3.0 Compatible

[ Edited ]

 

The port that is USB 3.0 is the same one that has Sleep and Charge. It has a lightning-bolt symbol near it.

 

          

 

PS..

 

Satellite P770  (PSBY3U-0X803N)

 

That model must be special order - or maybe for a big-box store. These are models in your part-number family (PSBY3U). They are very similar to yours. The same drivers and utilities should work.

 

Satellite P770-ST4NX2 (PSBY3U-09Y01N)

 

Satellite P770-ST4NX1 (PSBY3U-0C401N)

 

Satellite P775-S7234 (PSBY3U-02001D)

-Jerry
Channel 9

View solution in original post


All Replies
Posts: 46,770
Topics: 83
Kudos: 8,791
Solutions: 3,145
Registered: ‎12-04-2008

Re: Which Ports are USB 3.0 Compatible

Richard, you'll find a label on the bottom with the model number.

-Jerry
Channel 9
Member
Posts: 5

Re: Which Ports are USB 3.0 Compatible

[ Edited ]

I can find the Model Number  I was wondering which of the 4 USB ports 2 side  on left and 2 on right side are USB 3.0  compatible?

 

 

Posts: 46,770
Topics: 83
Kudos: 8,791
Solutions: 3,145
Registered: ‎12-04-2008

Re: Which Ports are USB 3.0 Compatible


I can find the Model Number


But you haven't told us yet.

-Jerry
Channel 9
Member
Posts: 5

Re: Which Ports are USB 3.0 Compatible

I believe you are referring to the Part No.

The Part Number is PSBY3U-0X803N

 

Posts: 46,770
Topics: 83
Kudos: 8,791
Solutions: 3,145
Registered: ‎12-04-2008

Re: Which Ports are USB 3.0 Compatible

[ Edited ]

 

The port that is USB 3.0 is the same one that has Sleep and Charge. It has a lightning-bolt symbol near it.

 

          

 

PS..

 

Satellite P770  (PSBY3U-0X803N)

 

That model must be special order - or maybe for a big-box store. These are models in your part-number family (PSBY3U). They are very similar to yours. The same drivers and utilities should work.

 

Satellite P770-ST4NX2 (PSBY3U-09Y01N)

 

Satellite P770-ST4NX1 (PSBY3U-0C401N)

 

Satellite P775-S7234 (PSBY3U-02001D)

-Jerry
Channel 9
Member
Posts: 5

Re: Which Ports are USB 3.0 Compatible

Thank You Jerry for your reply. You are correct I ordered this specific model with the specs I specifically requested.

 

 Again thanks for you reply,

and have a wonderful day.

 

Richard Colby

Posts: 46,770
Topics: 83
Kudos: 8,791
Solutions: 3,145
Registered: ‎12-04-2008

Re: Which Ports are USB 3.0 Compatible

You're welcome, Richard. Happy to help.

-Jerry
Channel 9
Member
Posts: 5

Re: Which Ports are USB 3.0 Compatible

Jerry,

 

   As a further confirmation that I found the USB 3.0 port with the lighting-bolt symbol, I also noticed that the tab used for the USB 3.0 port is Blue and slightly thicker than the USB 2.0 port that is a "gray" color if any color at all.

 

So look for lightening-bolt and the color blue (I think)

Richard Colby

Posts: 46,770
Topics: 83
Kudos: 8,791
Solutions: 3,145
Registered: ‎12-04-2008

Re: Which Ports are USB 3.0 Compatible

Ah, yes. I see that all over the place now. Thanks.

 

    

-Jerry
Channel 9
Posts: 21,713
Topics: 70
Kudos: 821
Solutions: 482
Registered: ‎10-04-2011

No USB 3.0 Port ? ?? Re: Which Ports are USB 3.0 Compatible

This thread has been moved to another message board. Click the link to jump to its new location.