Num Lock (P845)

Reply
Member
Posts: 6
Accepted Solution

Num Lock (P845)

I have a new Satellite P845 and cannot find how to activate the num lock. Man Sad I searched in the user's guide (the pdf file) but I could not find anything by entering keywords like lock, num lock etc. or looking at the F keys.

 

Can someone please tell me how to activate it?? I tried FN+F11 because I read somewhere that this is the way to activate the num lock on Satellite laptops, but it doesn't work with this model...

Thank you for your help!!

Paul

Posts: 47,020
Topics: 83
Kudos: 8,913
Solutions: 3,165
Registered: ‎12-04-2008

Re: Num Lock (P845)

Always tell us which Satellite P845 you have when you post here. There is a label on the bottom.

 

In the meantime..

 

You can toggle numlock by executing a tiny file. Download the attached Numlock.txt file. Change the .txt extension to .vbs, so the the file name becomes Numlock.vbs. If it's useful, you'll want to create a keyboard shortcut to execute it.

-Jerry
Channel 9

View solution in original post


All Replies
Posts: 1,735
Topics: 48
Kudos: 886
Solutions: 135
Registered: ‎10-22-2011

Re: Num Lock (P845)

[ Edited ]

Why would you need number lock on a keyboard that doesn't have a numberpad?

______________________________________________________
Qosmio X875 i7-3630QM, 32GB RAM, OCZ SSD Qosmio X505 i7-920XM, PM55, 16GB RAM, OCZ SSD
Satellite Pro L350 T9900, GM45, 8GB RAM , Intel 320 SSD (my baby) Satellite L655 i7-620M, HM55, 8GB RAM, Intel 710 SSD
Member
Posts: 6

Re: Num Lock (P845)

I need to insert ASCII characters sometimes and hoped I didn't have to open the character map or use "insert symbol" in Word (when I am using Word) every time. I thought there would be a way to do that. Usually in laptops it is possible to activate the number lock or the numper pad somehow. It is even possible with tiny netbooks...

Posts: 47,020
Topics: 83
Kudos: 8,913
Solutions: 3,165
Registered: ‎12-04-2008

Re: Num Lock (P845)

Always tell us which Satellite P845 you have when you post here. There is a label on the bottom.

 

In the meantime..

 

You can toggle numlock by executing a tiny file. Download the attached Numlock.txt file. Change the .txt extension to .vbs, so the the file name becomes Numlock.vbs. If it's useful, you'll want to create a keyboard shortcut to execute it.

-Jerry
Channel 9
Member
Posts: 6

Re: Num Lock (P845)

Thank you, I will do that.

And the model is P840/015. Sorry for the confusion, my father just bought it.

Posts: 47,020
Topics: 83
Kudos: 8,913
Solutions: 3,165
Registered: ‎12-04-2008

Re: Num Lock (P845)

 

Satellite P840/015 (PSPJ6A-015001)

 

Looking through your manual (attached), there does not appear to be a numlock function on that keyboard. That is, the keys are not shared that way. Are they?

-Jerry
Channel 9
Member
Posts: 6

Re: Num Lock (P845)

No, that's what surprised me. I thought there would be some sort of shortcut or hot key, but I could not find anything.

Member
Posts: 6

Re: Num Lock (P845)

OK, the only way I have found to do it is with the on-screen keyboard....

Posts: 47,020
Topics: 83
Kudos: 8,913
Solutions: 3,165
Registered: ‎12-04-2008

Re: Num Lock (P845)

If numlock is a valid state, the VBS file I supplied should toggle it when executed.

-Jerry
Channel 9
Member
Posts: 6

Re: Num Lock (P845)

I think so, but the on-screen keyboard should still be open. I pinned it to my taskbar now for easy access.