06-12-2010 07:15 AM
Hi there, am glad am in the community today, my profile is that I have a toshiba satellite pro, which I've the model been clean from the machine so it's not easy for me to read it to get the drivers for it, the only way is that I check the model from the dxdiag and it gives me only the toshiba satellite pro L300 only without the rest of the numbers to it, I want to know how can I get the model number of my laptop so that I can load the correct drivers for it.
Solved! Go to Solution.
06-12-2010 02:46 PM
06-21-2010 12:55 PM
Hi there I was able to get the info, from the link you gave me, I appericate it very well. I was able to read all the neccessary things I needed but there is still something missen thus I saw the model number alright but you know with toshiba you have to get the other remaining numbers which is if the model number is satellite pro L300, there should be another numbers which follows it but it didn't showed up like that. I want to know with the serial number only I will I be able to get the actual model?
06-21-2010 01:08 PM
Look in those utilities for a part number.
If it's a US machine, the number looks something like PSLB9U-00R011.
If it's a European machine, it's something like PSLB9E-02D00MG3.
06-25-2010
10:21 AM
- last edited on
06-25-2010
10:52 PM
by
Trina
Jerry this how my id is, so I was wondering if I could have the full drivers for it? Also in my look out I came across this website called driversagent.com which gives me the neccessary drivers needed for my updates including my scan id as well, I don't know if you know of this website?
TOSHIBA Satellite Pro L300 PSLB1E-020013EN
06-25-2010 10:52 AM
Satellite Pro L300-156 (PSLB1E-020013EN)
The Toshiba drivers and utilities for that European model are here.
Best to get them from Toshiba.
07-01-2010 09:50 AM
Hello Jerry, thanks so much for your help and time, I was able to get to where I wanted I never knew of this but I hope someday I will be able to help someone as well. Thanks.
07-01-2010 10:46 AM
You're welcome. Happy to help.
I hope someday I will be able to help someone as well.
That's what these forums are all about. There are forums for European users too.
Toshiba Support Forums in Europe
07-30-2010 04:17 PM
Mine is the L300-154, says so on plate on bottom of laptop. Part Number is there too.
05-19-2011 09:41 PM
Hi Jerry,
I've been looking for hours to find out if my laptop is a Satellite P200-ST2061 or Satellite P200-ST2071. This thread is my last hope.
I don't know how you found the answer for mohtaj but I ran the Belard Advisor and found out the laptop is a:
TOSHIBA Satellite P200 PSPBGU-0S7019
Can you tell me which version machine I have and where you found the info?
(I called Toshiba Suport but they didn't know either.)
Thanks very much!
- Rich
05-20-2011 06:05 AM
Satellite P200 (PSPBGU-0S7019)
Can you tell me which version machine I have..?
It doesn't work that way, Rich. Toshiba makes lots of special models for big box stores that do not appear separately here. Since the models in the same part-number family differ only in frills and software, it's sufficient to find one of those.
Compare your spec with that for the following model, which is in the same part-number family (PSPBGU).
Satellite P205-S6277 (PSPBGU-00W016)
Expect the drivers and utilities to be the same. They are here.
02-12-2013 12:10 AM
please can you help me finding the rivers for my laptop specially the display driver my model is c850d-b538 and thepart no is psc9uv-00r00ear thank you very much
Regards
02-12-2013 06:22 AM
eyasbad wrote:..
Please start a new thread for this.
Copyright © 2013 Toshiba America Information Systems, Inc. All rights reserved.