Connecting to a wireless router

Reply
Occasional Contributor
Posts: 19
Accepted Solution

Connecting to a wireless router

I have an older wireless router, the DLink DI-714P+ connected to a DSL modem, and would like my Satellite Pro L300D's wireless LAN to connect through it to the Internet. I do not see any instructions how to use the Atheros 802.11b/g wireless LAN on the laptop.

 

My router does have settings for wireless LAN and supports the 802.11b wireless network. The D-Link settings for the wireless access point are network ID(SSID), set to 'default', channel, set to '6', and security, set to 'None' with options for 'WEP','802.1','WPA-PSK', and 'WPA". There is also a page of wireless performance settings I can set in the D714P+ setup.

 

Any help hooking up my laptop to my wireless router so that it can access the Internet through the router would be most welcome. Thanks !

 

 


Accepted Solutions
Regular Advisor
Posts: 233

Re: Connecting to a wireless router


eldiener wrote:

I have an older wireless router, the DLink DI-714P+ connected to a DSL modem, and would like my Satellite Pro L300D's wireless LAN to connect through it to the Internet. I do not see any instructions how to use the Atheros 802.11b/g wireless LAN on the laptop.

 

My router does have settings for wireless LAN and supports the 802.11b wireless network. The D-Link settings for the wireless access point are network ID(SSID), set to 'default', channel, set to '6', and security, set to 'None' with options for 'WEP','802.1','WPA-PSK', and 'WPA". There is also a page of wireless performance settings I can set in the D714P+ setup.

 

Any help hooking up my laptop to my wireless router so that it can access the Internet through the router would be most welcome. Thanks !

 

 


Hi,

 

 

Satellite Pro L300D series is wifi capable . Here are the things that you need to do to connect to a wireless router.

 

. Check if Wireless Switch is on  ( for this system the on / off switch is located infront of the system aligned to the Audio jack )

. Click Start then go to Connect to

. Look for the name of your Router and Double click it.

 

 

Once it says connected. Try opening up Internet Explorer.

 

That should help you out connect to your routerSmiley Wink

________________________________________________________________________
"I'm Not the Message... Just the Messenger.. i Don't Play the Music... The music plays through me... Im just a Channel..... That's all I AM "

View solution in original post


All Replies
Regular Advisor
Posts: 233

Re: Connecting to a wireless router


eldiener wrote:

I have an older wireless router, the DLink DI-714P+ connected to a DSL modem, and would like my Satellite Pro L300D's wireless LAN to connect through it to the Internet. I do not see any instructions how to use the Atheros 802.11b/g wireless LAN on the laptop.

 

My router does have settings for wireless LAN and supports the 802.11b wireless network. The D-Link settings for the wireless access point are network ID(SSID), set to 'default', channel, set to '6', and security, set to 'None' with options for 'WEP','802.1','WPA-PSK', and 'WPA". There is also a page of wireless performance settings I can set in the D714P+ setup.

 

Any help hooking up my laptop to my wireless router so that it can access the Internet through the router would be most welcome. Thanks !

 

 


Hi,

 

 

Satellite Pro L300D series is wifi capable . Here are the things that you need to do to connect to a wireless router.

 

. Check if Wireless Switch is on  ( for this system the on / off switch is located infront of the system aligned to the Audio jack )

. Click Start then go to Connect to

. Look for the name of your Router and Double click it.

 

 

Once it says connected. Try opening up Internet Explorer.

 

That should help you out connect to your routerSmiley Wink

________________________________________________________________________
"I'm Not the Message... Just the Messenger.. i Don't Play the Music... The music plays through me... Im just a Channel..... That's all I AM "
Posts: 47,926
Topics: 85
Kudos: 9,130
Solutions: 3,230
Registered: ‎12-04-2008

Re: Connecting to a wireless router

I don't know if that router is compatible with Vista's wireless or not. Best to ask DLink.

 

Or maybe this applies:  Windows Vista cannot obtain an IP address from certain routers or from certain non-Microsoft DHCP se...

 

In the meantime, can you connect using an Ethernet cable t o the router?

-Jerry
Channel 9
Occasional Contributor
Posts: 19

Re: Connecting to a wireless router

That worked fine. Thanks !