Reply
Member
Posts: 2

l855-s5405 Specs

I cannot find any info of Toshiba Satellite L855-s5405 on site. I'm looking for the max ram and what voltage the dimm's run at. 

Member
Posts: 2

Re: l855-s5405 Specs

OK I found the ram specs for this model on another site

 

Toshiba Satellite L855-S5405 (PSKFUU-0RR004)

Memory Type: DDR3 PC3-12800, DDR3 PC3-14900, DDR3 (non-ECC)
Maximum Memory: 16GB
Slots: 2

Voltage 1.35v

Chipset: Intel HM76 chipset

Posts: 43,513
Topics: 73
Kudos: 6,294
Solutions: 2,896
Registered: ‎12-04-2008

Re: l855-s5405 Specs

 

Satellite L855-S5405 (PSKFUU-0RR004)

 

Apparently made for big-box stores like Best Buy.

 

Essentially the same as this model.

 

Satellite L855-S5112 (PSKFUU-008004)

 

I looked that up so I could refer you to the downloads here for possible future use.

-Jerry