Hello I am new to the forum and I have a question regarding Toshiba Satellite L775D-S7107
it initially has 4BG DDR3 RAM and my question is :
Can it be upgraded to 8GB DDR 3 RAM ? if so, do I need to purchase 2x chips with 4GB DDR3 Ram or a single 8GB chip ?
I would be grateful for some type of specification as for the RAM chip because there are different types of DDR 3
I have to point out that detailed tech specification on the official Toshiba page (spec in the .PDF file is showing error and cannot be previewed), therefore I do not know if max RAM memory may be increased or not based on basic description.