Reply
Member
Posts: 3

Toshiba L505 ES5018 MEMORY

Hi:
Can anyone help me with how much memory this laptop can handle? I am running W7 x64 and would like to get 8 megs installed, but I cannot find out if it can handle that amount. And Tosh does not give me that info in their spec sheets.

Thanks,

labans

Super Advisor
Posts: 1,472

Re: Toshiba L505 ES5018 MEMORY

[ Edited ]

Satellite L505 Detailed Product Specification1
Model Name: L505-ES5018 Part Number: PSLU0U-02S034 UPC: 883974369225
Configured with 3GB DDR3 800MHz (max 8GB)

 

Buy Kingston brand memory, it will work, other brands may not.

Welcome to the Toshiba user forums.
For those of you who do not know what a user forum is, it is a community of users who volunteer time to help other users. Anyone can participate. It's 100% voluntary.
Being super active is never a requirement
Occasional Advisor
Posts: 158

Re: Toshiba L505 ES5018 MEMORY

[ Edited ]

That would be 8GB.  Anything more than 4GB of RAM is severe overkill for about 95% of any possible applications you are going to use.  In that laptop, the gpu/cpu is going to be the bottleneck, not the lack of RAM.

 

The spec sheet I found indicates how much RAM it will handle:  L505-ES5018 Spec Sheet