12-10-2008 08:25 PM
Solved! Go to Solution.
12-11-2008 11:24 AM
12-11-2008 11:23 PM
Thanks for the driver link, I downloaded it and ran the file, it unzips and begins the installation and then fails - giving me the error: "Driver Installation Failed: Could not find the MEDIA device for this driver." Every time I boot up the laptop Windows XP sees the "PCI Device" and asks for a driver, allowing Windows to go online and search also turns up nothing - checking in device manager shows that all the audio codecs are installed, just no audio controller.
Any thoughts?
Thanks!
12-12-2008 05:58 AM
The Vista driver for your Satellite M305D-S4840 works for these computers..
Satellite M300-ST4060, M305-S4815, M305-S4819, M305-S4820, M305-S4822, M305-S4826, M305D-S4830, M305D-S4831, M305D-S48331, M305-S4860, M305D-S48441, M305-S4848, M305D-S4844, M305D-S4840, M305-S4835, M305D-S4833, M305D-S4828, M305D-S4829, P300-ST3014, P305D-S8816, P305D-S8818, P305-S8814, P305D-S8819, P305D-S8836, P305D-S8834, P305-S8842, P305-S8838, P305-S8832, P305-S8830, P305D-S8829, P305D-S8828, P305-S8826, P305-S88541, P305-S8854, P305-S8848, P305-S8857, P305D-S8845, P305-S8837, P305-S8844, P305D-S88361, P305-S8825, P305-S8824, P305-S8823, P305-S8822, P305-S8820, U400-ST5404, U405-S2820, U405-S2817, U405-SP2803, U405-S2856, U405D-S2848, U405-S2854, U405D-S2846, U405D-S2852, U405D-S2850, U405-S2833, U405-S2830, U405-S2824, U405-SP2801, U405-ST550W, U405D-S2870, U405-S2882, U405-S2878, U405D-S2874, U405D-S2863, U405-S2857, U405-S2826
Satellite Pro M300-EZ1001X, M300-S1002X, M300-EZ1001V, M300-S1002V, U400-S1001X, U400-SP2804C, U400-SP2908C, U400-SP2908R, U400-SP2908A, U400-SP2804R, U400-S1002V, U400-SP1801, U400-SP2804, U400-S1001V
Other Models All models having model/part numbers beginning in PSMD4U
The XP driver I gave you (driver_audio_conexant_os2008304a.exe) is provided for these machines..
Satellite P300-ST3014, P305-S8814, P305-S8820, P305-S8822, P305-S8825, P305-S8826, P305-S8832, P305-S8842, P305-S8837, P305-S8838, P305-S8830, P305-S8824, P305-S8823, U400-ST5404, U405-S2820, U405-S2817, U405-SP2803, U405-SP2801, U405-S2854, U405-S2833, U405-S2830, U405-S2824, U405-S2826
Satellite Pro M300-EZ1001X, M300-S1002X, M300-EZ1001V, M300-S1002V, U400-S1001X, U400-S1001V, U400-SP1801, U400-S1002V
Other Models All models having model/part numbers beginning in PSMD4U
Notice that some machines are on both lists. I can't explain why it didn't install.
Here's an earlier version that should work for the same reason...
driver_audio_conexant_27320D.exe
12-14-2008 09:03 PM
Hi again,
Thanks for the assistance... the second driver you gave me also did not work... same error message. However, upon checking again in the device manager, I saw that my sound card hardware had changed from "PCI Device" with a yellow question mark to "High Defintion Audio Bus" or something simular with a red X. I right clicked and enabled it and it went back to a yellow question mark. Then I installed again the first driver you gave me and this time it did not give the error and went into the setup menu and I was able to successfully install the driver. Everything is now working fine and I have audio.
Thanks again for the help!
12-14-2008 09:22 PM
Then I installed again the first driver you gave me and this time it did not give the error and went into the setup menu and I was able to successfully install the driver. Everything is now working fine and I have audio.
Thanks again for the help!
Happy to hear of your success! Thanks for giving us the details.
Copyright © 2013 Toshiba America Information Systems, Inc. All rights reserved.