11-18-2011 07:38 AM
I have been searching for hours to see what kind of upgrade I can do with my processor. I just ordered replacement memory so I can go to 8GB instead of 3GB and now want to see what is available for my CPU.
Currently this is what is on my laptop: (in case some of you don't know what comes with this model)
Windows 7 Home Pro - 64 Bit
AMD M880G Chipset
AMD Athlon II Dual Core P320 - 2.1 GHz, 1MB L2 Cache
The memory I ordered was 2 x 4GB DDR3 1333 PC3-10600
I'm sure someone out there can help me, because google hasn't been to friendly with me today.
11-21-2011 03:42 PM
CPU upgrades are not officially supported by Toshiba.
Of course, that doesn't mean it's not possible. Good luck!
11-21-2011 04:02 PM
ok, if you were running an intel processor, I could probably give you some options. Unfortunately, I have little experience with AMD, and haven't needed to research it.
This is where I always start. Look at the other L655D's that use the same chipset, but different CPU's. Make sure they are all the same socket type. Then compare the processors to see which is best. You can do a Yahoo search for the name of the processor and "benchmark". This is the best way to find the best processor that is known to work in your system.
Beyond that, you again research all CPU's that are the same socket and use the same chipset that you have in your computer. You run the risk of trying a CPU that may not work, but you may find one that works well and is better than anything installed from the factory.
I have had great luck with upgrading Intel chips in my laptops, but again, I started out with what was proven, and went from there.
12-16-2011 09:07 PM
12-16-2011 09:15 PM
OK. So CPU upgrades are not officially supported but I have a question about the design of the motherboard. Is the chip a solid part of the motherboard or does it plug in. I ask because I have heard that some laptops the CPU is a solid integration and is not really possible (with my knowledge) to upgrade. If it is not a plug in CPU is the mother board a plugin to the computer or is it hard wired in. I would assume that you would have this information about the4 product.
I also have a L655D - S5050.
12-17-2011 06:13 AM
your CPU is socketed. Some of the older laptops had hard soldered CPU's, and the netbooks with Intel Atom processors are hard soldered.
Copyright © 2013 Toshiba America Information Systems, Inc. All rights reserved.