Reply
Member
Posts: 1

L55-A5226 play Blue-Ray disc?

I just bought the Satellite L55-A5226 yesterday and was curious if it can play blue-ray movies?

Super Advisor
Posts: 1,936

Re: L55-A5226 play Blue-Ray disc?

[ Edited ]

Unless you ordered it with a bluray player it only shows DVD Drive on your spec sheet.

Fixed Optical Disk Drive7

DVD SuperMulti drive supporting 11 formats

o Maximum Read speed and compatibility: CD-ROM (24x), CD-R

(24x), CD-RW (16x), DVD-ROM (8x), DVD-R (8x), DVD-R DL

(6x), DVD-RW (6x), DVD+R (8x), DVD+R DL (6x), DVD+RW

(8x), DVD-RAM (5x)

Your support page is here :  http://support.toshiba.com/support/modelHome?freeText=1200005650

You will find all your specs, manuals, and downloads there.

 

You can use an external bluray player that connects with a usb on your laptop.

You can also double check by going to, start, control panel, device manager, then click on your dvd drive or if it list a bluray and  it will tell you CD, DVD, Bluray also.

S70-ABT2N22 Windows 7 Pro & 8.1Pro, C55-A5180 Windows 8.1****Click on White “Kudos” STAR to say thanks!****