Reply
Regular Contributor
Posts: 52

Install internal bluetooth

Morning fellas! Ok, here we go.

 

I have a P305D-S8834. What I want to do is install an internal bluetooth radio so I don't have to use a USB dongle, but I don't want to install it via one of the hubs so I don't lose the accessibility of that hub, that would defeat the purpose of installing it internally.

 

So I'm hoping that there is someone out there that has maybe done something similar to a unit such as mine, or at least tell me if it's feasible.

 

Thanks guys.

Satellite P305D-S8834
Windows 7 Ultimate 64 bit
AMD Turion X2 64
RADEON 3100 graphics
4 GHz DDR2 800, PC2-6400 RAM
2 Seagate 320GB 7200 rpm HDD