Reply
Occasional Contributor
Posts: 11
Accepted Solution

How to enter setup for a Satellite P755-S5390

Upon initially starting up my laptop, the options to enter the BIOS or the Setup are not displayed.  I have tried hitting 'esc' repeatedly but all that allows me to do is to run memory diagnostics or to start Windows 7 normally.  I have unseated and reseated the battery.  Nothing seems to help.  When I first purchased the laptop a couple of weeks ago, I know the options were displayed, but they do not show up now.  All I want to do is to go through the settings in the BIOS and to make sure they are set for optimization.  Thanks for all suggestions.

 

Model:  Toshiba Satellite P755-S5390

OS:  Windows 7

Frequent Advisor
Posts: 1,463

Re: How to enter setup for a Satellite P755-S5390

Try F2, that should work.

______________________________________________________
Qosmio X875 i7-3630QM, 32GB RAM, OCZ SSD Qosmio X505 i7-920XM, PM55, 16GB RAM, OCZ SSD
Satellite Pro L350 T9900, GM45, 8GB RAM , Intel 320 SSD (my baby) Satellite L655 i7-620M, HM55, 8GB RAM, Intel 710 SSD (travel system)
Ace Advisor
Posts: 41,725

Re: How to enter setup for a Satellite P755-S5390

[ Edited ]

 

Satellite P755-S5390 

 

 

In case neither F1 nor F2 works: When Fast Boot is enabled, you must first hold down the F2 key and then power-on the computer.

 

BTW, you can also reach Setup this way while Windows runs.

 

   Start > All Programs > Toshiba > Utilities > HWSetup

-Jerry
Occasional Contributor
Posts: 11

Re: How to enter setup for a Satellite P755-S5390

Thanks Jerry.  Holding down F2 & powering on the system worked great.  I really appreciate the help.

Member
Posts: 1

Re: How to enter setup for a Satellite P755-S5390

It worked for me too, Jerry.. Thank you very much!!!

Ace Advisor
Posts: 41,725

Re: How to enter setup for a Satellite P755-S5390

Happy to help you, Frank.

-Jerry