Reply
Member
Posts: 4

How I installed windows 7 on a Satellite C855D-S5315

First I thought the pos had hardware failure because none of my bootable dvds and flash drive was working. Then, I remembered about secure boot (which is dumb to enable by default cos not everyone knows about it and would buy replacement hardware they dont need).... So I booted into bios, and sure enough it was enabled. So I disabled secure boot, and changed boot mode from UEIF to CSM which solved my boot fail problem.

 

So after I installed windows 7 64bit, there was 4 devices missing drivers according to device manager. Since most manufacturers support website has been helpful in the past when it comes to installing drivers I decided to try toshiba's support site first. it was not as user-friendly as the others. But I did manage to find 1 driver I needed on it. The other 3 I found on realtek and dell's driver support site after looking up device id using pcidatabase.

 

I saved them to google drive so next time it wont take so long, decided to share in case anyone else was having problems finding drivers for windows 7 64bit on a Satellite C855D-S5315

 

ethernet: https://drive.google.com/folderview?id=0B_-BKmXr1ljJLTdQMFF5WkphVjg&usp=sharing

 

cardreader: https://docs.google.com/file/d/0B_-BKmXr1ljJVXl0YmtabFNMdXc/edit?usp=sharing

 

wireless/wif: https://docs.google.com/file/d/0B_-BKmXr1ljJMkw1cFFmckp6YTA/edit?usp=sharing

 

smbus: https://docs.google.com/file/d/0B_-BKmXr1ljJQWxLN2pnb1pmRUk/edit?usp=sharing


According to device manager, after I installed those 4 drivers, there was no more missing drivers.


hope this helps

Posts: 43,168
Topics: 71
Kudos: 6,008
Solutions: 2,862
Registered: ‎12-04-2008

Re: How I installed windows 7 on a Satellite C855D-S5315

 

Satellite C855D-S5315 (PSCBQU-00F009)

 

Thank you for the drivers!

 

Those should work for all computers in part-number family PSCBQU - probably a bunch.

-Jerry
Member
Posts: 1

Re: How I installed windows 7 on a Satellite C855D-S5315

i have satelliteL500 that wont load past toshiba page can get into bios sometimes tried to install windows xp from cd seemed to work then when tried to use it next time i am stuck in limbo. dont care if u can help me install start-up from disc or original setting would just like to beable to use my laptop    thx erica

Member
Posts: 4

Re: How I installed windows 7 on a Satellite C855D-S5315

no problem, glad to help when I can, windows 8 came pre-installed on the C855D-S5315 and cousin wanted windows 7... figured there might be more people out there who wanted to downgrade from 8 to 7 too but couldnt find the drivers so decided to share them since i was already saving them for myself on google drive

 

not sure if anyone even needed help finding win7 drivers for this laptop but it only took a second to post in case they do. 

 

Also, after I posted this thread, I noticed screen saver wouldnt work because of poor video or something (forgot what the error msg said) so I decided to try an install a video card even though device manager did not list my video card as missing drivers..... 

 

1. First I googled C855D-S5315, and looked up the graphic/video card model from the cnet page.

 

2. Then I googled "AMD Radeon HD 6310M" AND driver "windows 7" for the download link.

 

-- download page: http://support.lenovo.com/en_US/downloads/detail.page?DocID=DS030424

-- download link: http://download.lenovo.com/ibmdl/pub/pc/pccbbs/mobiles/hnd602ww.exe

 

lenovo support page came up as first results so I just went with it. Despite device manager not saying my video card was missing drivers, I think it really was, cos after I installed this driver I was able to use screensaver again 

I don't know if laptop is missing anymore drivers that device manager failed to list but I dont think it is 

 

Member
Posts: 4

Re: How I installed windows 7 on a Satellite C855D-S5315

@ericabiagioni - sorry, i'm not sure what the problem is, you might have better luck if you try posting a new thread in the trouble shooting category of this forum. 

 

try this page: http://forums.toshiba.com/t5/forums/postpage/board-id/brd_gen

 


From what I read, it sounds like hardware failure, but i'm not a PC Expert or anything. A few things I would try...

 

1. Make sure its plugged in to a working electrial outlet. My sister onced called me because she didn't know her computer was unplugged and wondered why it wasnt working

2. while plugged in, remove the battery, and try an use it. I've fixed 2 laptops that would not turn on just by removing the battery. 

 

3. Try an use the computer with a Ubuntu Live CD/Flashdrive. If your harddrive is the problem, you can find out by using a live cd because it boots from a flash drive or cd instead of harddrive.

Posts: 43,168
Topics: 71
Kudos: 6,008
Solutions: 2,862
Registered: ‎12-04-2008

Re: How I installed windows 7 on a Satellite C855D-S5315

[ Edited ]

For those downgrading computers in part-number family PSCBQU..

 

According to this message, you should also take a look at this blog.

 

   How to downgrade the Toshiba Satellite C855D-S5320 laptop from Windows 8 to Windows 7

-Jerry
Member
Posts: 1

Re: How I installed windows 7 on a Satellite C855D-S5315

You Sir are a life saver! thank you so very much Robot tongueHeart