12-05-2008 11:52 PM
Hello,
I have a Satellite P205-S6307 using Vista. I recently tried to use my headphone jack to listen to a video, but I get no sound. When I plug in the headphones, I don't even get static. These headphones do not have a volume switch. However, they work fine on other computers. Also, when I do plug them in, the computer speakers still play and don't shut off. I've checked all the settings that I can find that relate to audio speakers-headphones etc. but nothing works.
I'd appreciate any suggestions.
Thanks
ST
12-07-2008 06:29 AM
12-07-2008 08:39 PM
Hello,
Thanks for the reply. Yes it did work! But only briefly. If I unplugged the headphones and then replugged them in they wouldn't work and neither would the laptop speakers. Then I could reset he default and the laptop speakers would work again.
I at least got it to work some. That's more than I've ever been able to do.
Thank you again,
ST
12-07-2008 11:16 PM
Nice to see you up and running now !
Cheers !
Copyright © 2013 Toshiba America Information Systems, Inc. All rights reserved.