07-24-2010 05:30 PM
So i enabled Fast boot .. nice feature ,, PC boots Quicker
,,, But now i can't seem to Enter the Bios ,,,, Any Clues as to how it's done now that fast boot is enabled ? ![]()
Solved! Go to Solution.
07-24-2010 06:32 PM
OK, found the Fix in the Manual .. lol ...
Click Start, All Programs, TOSHIBA, Utilities, and then HWSetup ..
Kinda Kool That i can adjust Bios Settings from within Windows ![]()
07-27-2010 07:47 PM
You can also hold down the ESC key and then power on.
It should take you to the BIOS Setup. This is what you do if you hard disk crashed.
07-27-2010 08:07 PM
Tried that.... didnt work
07-28-2010 02:47 PM
I am so sorry, it is the F2 key.
Hold down the F2 key and then power on. I just tried it and it worked.
Again, I am sorry for the miss information.
07-28-2010 06:37 PM - edited 07-28-2010 06:39 PM
OK kool, that worked.... Ok problem is when i use fast boot the internal mic is disabled for some strange reason ...
07-29-2010 10:31 AM
Let me try that on my machine. I will get back to you.
08-12-2010 05:47 PM
I just tried that.
Sure enough the mic is out. This only happens when in Fast Boot. I spoke to Support, I got through, they are investigating it. If I find a solution I will post it here.
Good luck,
08-12-2010 07:25 PM
Kool thanks ... hope they release a patch/fix soon ...
09-18-2011 12:35 PM
Just a note that I just did a Bios Update and the Microphone issue is Fixed..
The mic now works even when fast boot is enabled.. ![]()
04-19-2013 06:12 AM
Pres and hold F12 and power button until display boot menu. now select setup.
Copyright © 2013 Toshiba America Information Systems, Inc. All rights reserved.