Reply
Occasional Contributor
ACDC
Posts: 15
0
Accepted Solution

ACPI Flash BIOS version 3.10 for Satellite/Pro L655/L750/L755 (PSK1W/PSK1X/PSK2Y)(v3.10)

Just want to verify if this BIOS is compatible with my L755-S5217 BIOS.I've read a lot about failed BIOS updates for Satellite laptops so I do'nt update it using the earlier releases.By the way my BIOS is currently version 2.0 i'm afraid i'm gonna mess with my laptop.

Moderator
Peter
Posts: 10,179
0

Re: ACPI Flash BIOS version 3.10 for Satellite/Pro L655/L750/L755 (PSK1W/PSK1X/PSK2Y)(v3.10)

I assume you mean S5271, not S5217. Unfortunately, you didn't link to a particular download. You linked to the general support page for that product. However, yes, the BIOS listed on a model's support page should be compatible with it. Even so, I would recommend you do not update unless you need to update it to fix an on-going issue.

- Peter
Member
CODave
Posts: 1
0

Re: ACPI Flash BIOS version 3.10 for Satellite/Pro L655/L750/L755 (PSK1W/PSK1X/PSK2Y)(v3.10)

Hi,I just got that same msg and I was questioning that myself.Good to know that I don't have to accomplish unless I'm having issues.

 

  CODave

Occasional Contributor
ACDC
Posts: 15
0

Re: ACPI Flash BIOS version 3.10 for Satellite/Pro L655/L750/L755 (PSK1W/PSK1X/PSK2Y)(v3.10)

it's S5217 but it's not listed in the product support of toshiba.yes i dont have any issues so thank you very much Peter now i know that i dont need to update my BIOS.
Moderator
Peter
Posts: 10,179
0

Re: ACPI Flash BIOS version 3.10 for Satellite/Pro L655/L750/L755 (PSK1W/PSK1X/PSK2Y)(v3.10)

[ Edited ]

ACDC, if you give me your part number (which should also be on the bottom of your laptop), I should be able to get you the link to your model's support page (in case you need it in the future).

- Peter
Occasional Contributor
ACDC
Posts: 15
0

Re: ACPI Flash BIOS version 3.10 for Satellite/Pro L655/L750/L755 (PSK1W/PSK1X/PSK2Y)(v3.10)

Peter my Part number is PSK1WU-08J004

Ace Advisor
Jerry_Lippey
Posts: 33,049
0

Re: ACPI Flash BIOS version 3.10 for Satellite/Pro L655/L750/L755 (PSK1W/PSK1X/PSK2Y)(v3.10)

 

Satellite L755-S5217 (PSK1WU-08J004)

 

Satellite L755-S5271 (PSK1WU-06W004)

 

Because they are in the same part-number family (PSK1WU), the downloads should be the same.

-Jerry