Reply
Occasional Contributor
Posts: 12

Satellite A205-S5000 Cannot connect internet

[ Edited ]

Satellite A205-S5000 Cannot connect internet(wireless)

Other computers are workin fine.

 

-Network and Sharing center is Local and Internet

-Ping google.com received 4 replies

-but when open IE, its just searching homepage and nothing happens.

-Proxy is disabled

-Restarted DCHP client service

-Reset IE7 settings

 

 

Overall still not working.

Help?

Message Edited by ZeroConfig on 12-14-2008 05:45 PM
Regular Advisor
Posts: 233

Re: Satellite A205-S5000 Cannot connect internet


ZeroConfig wrote:

Satellite A205-S5000 Cannot connect internet

-Network and Sharing center is Local and Internet

-Ping google.com received 4 replies

-but when open IE, its just searching homepage and nothing happens.

-Proxy is disabled

-Restarted DCHP client service

-Reset IE7 settings

 

Overall still not working.

Help?


 

 

Hi there,

 

Are you Connecting to  a Wired or Wireless connection ?

________________________________________________________________________
"I'm Not the Message... Just the Messenger.. i Don't Play the Music... The music plays through me... Im just a Channel..... That's all I AM "
Ace Advisor
Posts: 41,959

Re: Satellite A205-S5000 Cannot connect internet


Cannot connect internet(wireless)

 

What happens when you try to connet via Ethernet cable?

 

Troubleshooting always starts with the simplest configuration.

-Jerry
Occasional Contributor
Posts: 12

Re: Satellite A205-S5000 Cannot connect internet

Its a wireless connection.

It works with wired.

 

 

Ace Advisor
Posts: 41,959

Re: Satellite A205-S5000 Cannot connect internet

You say that you can browse the web when connected with a cable and you can ping google.com when connected with wireless, but you cannot browse with the wireless connection? Have I got it right?

 

That's really hard for me to imagine!

 

Is this something new? Did it ever work properly?

 

Any other symptoms?

-Jerry
Occasional Contributor
Posts: 12

Re: Satellite A205-S5000 Cannot connect internet

again no problem with wired connection

Its just on wireless, i cannot browse IE its page cannot be displayed.

but its getting replies pinging google.com

 

 

Ace Advisor
Posts: 41,959

Re: Satellite A205-S5000 Cannot connect internet

You didn't answer this part...

  

    Is this something new? Did it ever work properly? Any other symptoms?

 

Do you have other Vista machines connected to this router via wireless?

 

I suspect the router (even though it handles other machines properly). It wouldn't hurt to cycle power on the router.

-Jerry
Occasional Contributor
Posts: 12

Re: Satellite A205-S5000 Cannot connect internet

It was a able to connect wireless to a hotspot.

Issue might be something with the wireless router.

Desktop PC connected to the router using ethernet cable.

This is the only wireless laptop connected.

Ace Advisor
Posts: 41,959

Re: Satellite A205-S5000 Cannot connect internet

What's the make and model of the router?

 

Does the desktop run Vista?

 

Many older routers do not handle Vista properly. Some of the more recent ones even need firmware upgrades.

-Jerry