04-01-2012 04:49 AM
When my computer is in sleep mode and I open the lid, my computer wakes up automatically. I would like to disable this feature but instead manually press the power button for the computer to wake up.
Toshiba Satellite A215-S4757
Windows 7 Ultimate
Processor: AMD Turion(tm) 64 X2 Mobile Technology TL-56 1.80 GHz
Installed memory (RAM): 2.00 GB (1.87 GB usable)
System type: 32-bit Operating System
Solved! Go to Solution.
04-01-2012 07:30 AM
Go to Control Panel/Power Options and click on "Choose what the Power Button does" in the left pane and make your selections. Be sure and click on "Save Changes" before you close.
C.B.
04-01-2012 11:22 AM
Thanks for your reply but this is not what I wanted. In Power Options I can only choose what the power button does only when the computer is awake. However, what I want is whilst the computer is in sleep mode, the computer resumes only when I press the power button and not when I open the lid.
04-01-2012 11:49 AM
In Power Options, for "Closing Lid", select "Do Nothing". Then, select for "Power Button", "Sleep". Then, put it to sleep by pressing the Power Button or by FN+F3. Then, wake it up by pressing the Power Button as you desire. It will NOT wake up just by raising the lid.
C.B.
04-02-2012 08:11 AM
cbwilsha wrote:[...] It will NOT wake up just by raising the lid.
C.B.
But, unfortunately, my laptop DOES wake up when I raise the lid.
04-02-2012 08:50 AM
When I follow my instructions on my 3 Toshiba's, they do NOT wake up when raising the lid so I don't know of anything else to suggest to you.
C.B.
04-02-2012 02:54 PM - edited 04-03-2012 05:47 PM
I just tried it on a A215-S4817 that I have here, and it worked no problem.
If you REALLY want to disable it, you can remove the magnet in the display bezel. It is just to the left of the Webcam if you have one. Just remove the 4 or 6 screws(whichever model you have) that hold the bezel in place, slowly pry it away, and remove the magnet. The down side to this is that it will no longer hibernate when you close the screen. You would HAVE to remember to tell it to hibernate.
04-03-2012 02:50 AM
Thanks for your help.
04-03-2012 02:51 AM
I would like to thank you alot for help! It totally worked.
04-03-2012 07:22 AM
I'm glad you solved your problem, cb93 and thanks a lot for reposting with the picture so others will be helped also. I learned something new from drev9 myself and thank him for that.
C.B.
04-03-2012 09:14 AM
No problem!
On almost all of the Toshiba laptops I have worked on, you can find the placement of the magnet by running a screwdriver along the top edge of the bezel until you feel the magnet pull it in. Glad it helped.
Copyright © 2013 Toshiba America Information Systems, Inc. All rights reserved.