Reply
Member
Posts: 2

C55-A5300 boot from USB

Having a real issue with my laptop not wanting to boot from USB.

 

Steps taken:

    1. Disabled security boot (option doesnt show up with CSM boot?)

    2. Made sure Fast Boot is disabled

    3. Switched from UEFI to CSM boot

    4. Updated firmware (1.2o)

    5. Am using F12 to select my media to boot from

 

Am able to boot from media on another device.

Member
Posts: 2

Re: C55-A5300 boot from USB

I said screw it to the USB installation.

 

Popped the HD into my desktop.

 

http://www.instructables.com/id/Install-Windows-7-without-USB-or-DVD-without-upgra/

Posts: 2,195
Topics: 28
Kudos: 1,058
Solutions: 119
Registered: ‎07-26-2013

Re: C55-A5300 boot from USB

Nice, thanks for posting your solution.

S70-ABT2N22 Windows 7 Pro & 8.1Pro, C55-A5180 Windows 8.1****Click on White “Kudos” STAR to say thanks!****
Occasional Contributor
Posts: 15

Re: C55-A5300 boot from USB

this seems like a major issue with the latest 1.1 bios release.   see this thread

http://forums.toshiba.com/t5/Satellite-Laptops-all-other/Trouble-with-Satellite-C55-A5104-Activating...