problem with toshiba satellite a300

Reply
Member
Posts: 3

problem with toshiba satellite a300

I have a TOSHIBA satellite A300 Laptop  after I install a fresh Windows 7 version on my laptop and after downloading all necessary drivers I have this problems : 

sometimes when I turn on the laptop ... the resolution is automatically set to 800X600 and both the touch pad and keyboard are not working ( freeze) then after I restart it ... every thing back normally ...

and also my friend have the same problem with his laptop

Posts: 47,010
Topics: 83
Kudos: 8,911
Solutions: 3,164
Registered: ‎12-04-2008

Re: problem with toshiba satellite a300

Which Satellite A300? There is a label on the bottom.

-Jerry
Channel 9
Member
Posts: 3

Re: problem with toshiba satellite a300

psag0e 

Posts: 47,010
Topics: 83
Kudos: 8,911
Solutions: 3,164
Registered: ‎12-04-2008

Re: problem with toshiba satellite a300

 

The model designation looks something like Satellite A300-1J1, and the part number something like PSAG0E-03U01YEN.

 

According to this bulletin, Toshiba does not support Windows 7 on the Satellite A300. So don't be surprised if things don't go well.

 

   Windows 7 upgrade: Toshiba Supported Laptop Models

 

In any case, get the drivers and utilities for that laptop from here.

 

Use 32-bit Windows 7, and be sure to install the chipset and display drivers prior to any others.

-Jerry
Channel 9