Toshiba Satellite A665-11Z Reboot Error

Reply
Member
Posts: 1

Toshiba Satellite A665-11Z Reboot Error

I recently had my fan replaced and decided to reboot my laptop and during the process of the CRC File after the first part of the reboot was successful, it gave me a error and told me to restart which I did so and then after the starting windows bit, during the 'Setup is starting services' bit, it gives me this error:

 

"The Computer restarted unexpectedly or encounter an unexpected error. Winsdows installation cannot proceed. To install Windows, click OK to restart the computer and then restart the installation."

 

This continues to occur every restart in a loop. Can anyone help me what I do need to do to stop this and to successfully reboot without any of these dumb problems

 

Thanks in Advance

Posts: 21,719
Topics: 70
Kudos: 852
Solutions: 483
Registered: ‎10-04-2011

Re: Toshiba Satellite A665-11Z Reboot Error

Is that a European model? You'll want to check on the site for Toshiba of Europe. This site only supports the US market.

- Peter
Posts: 48,242
Kudos: 9,203
Solutions: 3,265
Registered: ‎12-04-2008

Re: Toshiba Satellite A665-11Z Reboot Error

 

Satellite A665-11Z (PSAW3E-05K00TEN)

 

Turn the computer on and immediately press and hold the F8 key.

 

On the Advanced Boot Options menu, choose Repair Your Computer.

 

When you reach the System Recovery Options menu, choose Startup Repair.

-Jerry
Channel 9