How do I restore to factory settings if the hard drive is completely wiped?

Reply
Member
Posts: 3

How do I restore to factory settings if the hard drive is completely wiped?

[ Edited ]

Hello, I just bought two A665-S6050 models and both hard drives are completely wiped, no restore partition. I have windows to load and both have keys. How can I make these to factory condition without purchacing the serial specific restore disks from toshiba? Or do you think these would sell and perform better with just a clean install + necessary drivers? I'm not all that familiar with what Toshiba utilities are out there or which to use. Thanks, curious on your opinions

Posts: 48,228
Kudos: 9,197
Solutions: 3,265
Registered: ‎12-04-2008

Re: How do I restore to factory settings if the hard drive is completely wiped?

 

Satellite A665-S6050

 

Order the recovery discs from Toshiba.

 

   Order Toshiba Recovery Media

 

See the section Restoring from recovery DVDs/media, which begins on p. 73 of the User's Guide.

 

   Satellite A660 Series User’s Guide

-Jerry
Channel 9