How do I disable auto-resume when I open the lid?

Reply
Member
Posts: 5
Accepted Solution

How do I disable auto-resume when I open the lid?

When my computer is in sleep mode and I open the lid, my computer wakes up automatically. I would like to disable this feature but instead manually press the power button for the computer to wake up.

Toshiba Satellite A215-S4757
Windows 7 Ultimate

Processor: AMD Turion(tm) 64 X2 Mobile Technology TL-56 1.80 GHz
Installed memory (RAM): 2.00 GB (1.87 GB usable)
System type: 32-bit Operating System

Posts: 1,735
Topics: 48
Kudos: 886
Solutions: 135
Registered: ‎10-22-2011

Re: How do I disable auto-resume when I open the lid?

[ Edited ]

I just tried it on a A215-S4817 that I have here, and it worked no problem. 

 

If you REALLY want to disable it, you can remove the magnet in the display bezel.  It is just to the left of the Webcam if you have one.  Just remove the 4 or 6 screws(whichever model you have) that hold the bezel in place, slowly pry it away, and remove the magnet.  The down side to this is that it will no longer hibernate when you close the screen.  You would HAVE to remember to tell it to hibernate.

______________________________________________________
Qosmio X875 i7-3630QM, 32GB RAM, OCZ SSD Qosmio X505 i7-920XM, PM55, 16GB RAM, OCZ SSD
Satellite Pro L350 T9900, GM45, 8GB RAM , Intel 320 SSD (my baby) Satellite L655 i7-620M, HM55, 8GB RAM, Intel 710 SSD

View solution in original post


All Replies
Posts: 4,848
Topics: 57
Kudos: 1,617
Solutions: 377
Registered: ‎05-03-2009

Re: How do I disable auto-resume when I open the lid?

Go to Control Panel/Power Options and click on "Choose what the Power Button does" in the left pane and make your selections. Be sure and click on "Save Changes" before you close.

 

C.B.

C.B.

Toshiba Sat. C75D-B7260 Win 8.1 64 Bit--Toshiba Sat. L775D-S7132 Win 10 Home RTM Upgrade from W7 and Win 10 PRO Insider Preview--Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit--Toshiba Sat. Radius P25W-C2300-4K Win 10 Home 64 Bit
Member
Posts: 5

Re: How do I disable auto-resume when I open the lid?

Thanks for your reply but this is not what I wanted. In Power Options I can only choose what the power button does only when the computer is awake. However, what I want is whilst the computer is in sleep mode, the computer resumes only when I press the power button and not when I open the lid.

Posts: 4,848
Topics: 57
Kudos: 1,617
Solutions: 377
Registered: ‎05-03-2009

Re: How do I disable auto-resume when I open the lid?

In Power Options, for "Closing Lid", select "Do Nothing". Then, select for "Power Button", "Sleep".  Then, put it to sleep by pressing the Power Button or by FN+F3. Then, wake it up by pressing the Power Button as you desire. It will NOT wake up just by raising the lid.

 

C.B.

C.B.

Toshiba Sat. C75D-B7260 Win 8.1 64 Bit--Toshiba Sat. L775D-S7132 Win 10 Home RTM Upgrade from W7 and Win 10 PRO Insider Preview--Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit--Toshiba Sat. Radius P25W-C2300-4K Win 10 Home 64 Bit
Member
Posts: 5

Re: How do I disable auto-resume when I open the lid?


cbwilsha wrote:

[...] It will NOT wake up just by raising the lid.

 

C.B.


But, unfortunately, my laptop DOES wake up when I raise the lid.

Posts: 4,848
Topics: 57
Kudos: 1,617
Solutions: 377
Registered: ‎05-03-2009

Re: How do I disable auto-resume when I open the lid?

When I follow my instructions on my 3 Toshiba's, they do NOT wake up when raising the lid so I don't know of anything else to suggest to you.

 

C.B.

C.B.

Toshiba Sat. C75D-B7260 Win 8.1 64 Bit--Toshiba Sat. L775D-S7132 Win 10 Home RTM Upgrade from W7 and Win 10 PRO Insider Preview--Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit--Toshiba Sat. Radius P25W-C2300-4K Win 10 Home 64 Bit
Posts: 1,735
Topics: 48
Kudos: 886
Solutions: 135
Registered: ‎10-22-2011

Re: How do I disable auto-resume when I open the lid?

[ Edited ]

I just tried it on a A215-S4817 that I have here, and it worked no problem. 

 

If you REALLY want to disable it, you can remove the magnet in the display bezel.  It is just to the left of the Webcam if you have one.  Just remove the 4 or 6 screws(whichever model you have) that hold the bezel in place, slowly pry it away, and remove the magnet.  The down side to this is that it will no longer hibernate when you close the screen.  You would HAVE to remember to tell it to hibernate.

______________________________________________________
Qosmio X875 i7-3630QM, 32GB RAM, OCZ SSD Qosmio X505 i7-920XM, PM55, 16GB RAM, OCZ SSD
Satellite Pro L350 T9900, GM45, 8GB RAM , Intel 320 SSD (my baby) Satellite L655 i7-620M, HM55, 8GB RAM, Intel 710 SSD
Member
Posts: 5

Re: How do I disable auto-resume when I open the lid?

Thanks for your help.

Member
Posts: 5

Re: How do I disable auto-resume when I open the lid?

I would like to thank you alot for help! It totally worked.

 


Posts: 4,848
Topics: 57
Kudos: 1,617
Solutions: 377
Registered: ‎05-03-2009

Re: How do I disable auto-resume when I open the lid?

I'm glad you solved your problem, cb93 and thanks a lot for reposting with the picture so others will be helped also. I learned something new from drev9 myself and thank him for that.

 

C.B.

C.B.

Toshiba Sat. C75D-B7260 Win 8.1 64 Bit--Toshiba Sat. L775D-S7132 Win 10 Home RTM Upgrade from W7 and Win 10 PRO Insider Preview--Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit--Toshiba Sat. Radius P25W-C2300-4K Win 10 Home 64 Bit
Posts: 1,735
Topics: 48
Kudos: 886
Solutions: 135
Registered: ‎10-22-2011

Re: How do I disable auto-resume when I open the lid?

No problem!

 

On almost all of the Toshiba laptops I have worked on, you can find the placement of the magnet by running a screwdriver along the top edge of the bezel until you feel the magnet pull it in.  Glad it helped.

______________________________________________________
Qosmio X875 i7-3630QM, 32GB RAM, OCZ SSD Qosmio X505 i7-920XM, PM55, 16GB RAM, OCZ SSD
Satellite Pro L350 T9900, GM45, 8GB RAM , Intel 320 SSD (my baby) Satellite L655 i7-620M, HM55, 8GB RAM, Intel 710 SSD