Hard drive has bad sectors

Occasional Contributor
Posts: 11

Hard drive has bad sectors

I have an A505-S6033 with a Hitachi HTS545050B9A300 hard drive. When I try to run chkdsk it says it has bad sector or errors on the drive. I tell it to run a scheduled drive scan on start up and it never does it. I cannot figure out how to fix this. I have even reformatted the drive and reinstalled my OS. It fixes nothing. Hitachi has a download tool to scan the drive but it's not compatible with Windows 7 64-bit operating systems.

Can anybody help me with this problem?

All Replies
Super Advisor
Posts: 1,472

Re: Hard drive has bad sectors

Replace the hard drive.  If the unit is under warranty, contact Toshiba and arrange to have it serviced.


When a hard drive begins showing bad sectors, it is best to replace it ASAP, or you risk losing all of the data on the drive.

Welcome to the Toshiba user forums.
For those of you who do not know what a user forum is, it is a community of users who volunteer time to help other users. Anyone can participate. It's 100% voluntary.
Being super active is never a requirement