08-03-2011 09:24 AM
I may be interested in replacing the original SSD on my Qosmio x505 q890 with a larger, faster SSD (say 256GB and SATA 3). I have three related questions:
1. Which, if any, 256GB SSDs are compatible with the X505 Q890?
2. Can the q890 take advantage of the faster SATA 3 transfer speeds?
3. What is the most efficient means for cloning the existing SSD (Win 7 Pro OS) to the new SSD before replacing it?
Many thanks for your help!
Kim
08-03-2011 05:13 PM
Yes, you can upgrade the hard drive to a larger SSD drive.
I use Nortons Ghost to copy the system and all files on the drive to a new drive.
08-10-2011 07:18 AM
I have the same issue as Kim. Anybody know the answer to her other questions?
What brand?
What technologies are compatible?
Does a bigger/faster SSD overheat?
08-10-2011 12:02 PM - edited 08-10-2011 12:03 PM
klshome wrote:I may be interested in replacing the original SSD on my Qosmio x505 q890 with a larger, faster SSD (say 256GB and SATA 3). I have three related questions:
1. Which, if any, 256GB SSDs are compatible with the X505 Q890?
2. Can the q890 take advantage of the faster SATA 3 transfer speeds?
3. What is the most efficient means for cloning the existing SSD (Win 7 Pro OS) to the new SSD before replacing it?
Many thanks for your help!
Kim
1. Any SSD that is SATA II or below will work. SATA III may also work if it is backwards compatible (probably is). But your laptop will not get SATA III speeds.
2. No. The q890 is baed on the HM55 chipset (comes with i7-720qm or i7-740qm CPU). The HM55 chipset is technologically limited to SATA II.
The HM65 is the next generation Intel chipset that comes with Sandy Bridge CPUs (i7-2630QM); HM65 was released January of 2011. Sandy Bridge (HM65) can do SATA III speeds. For example, the x505 q8100X series (and x775 series) were the first lines of Qosmios to include the HM65 chipset.
3. No idea. I have heard some SSD drives come with cloning software to help you. Could also try using your System Restore Discs to reinstall your OS on the SSD.
Good luck and keep us updated with your results.
Copyright © 2013 Toshiba America Information Systems, Inc. All rights reserved.