Reply
Regular Advisor
Squall_Rinoa89
Posts: 204
0

Re: Qosmio w NVIDIA 460M can run Dragon Age 2 at Max Settings!


daveharris118 wrote:

Semi-hard to believe this as I had heard that DA2 pushed at GTX 580 pretty hard...


The issues were hammered out with nVidia Display Driver fixes. DA2 is NOT by far a demanding game. Just a porely optimized game that is now fixed when EA worked with nVidia to fix the driver problems.

ex Toshiba Qosmio X305-Q701 Owner
Toshiba Satellite A665-3DV10 Owner
PSN: Squall_Rinoa89
I DON'T SUGAR COAT STUPIDITY
Regular Advisor
alexuw
Posts: 294
0

Re: Qosmio w NVIDIA 460M can run Dragon Age 2 at Max Settings!

Toshiba just came out with an nvidia driver: 296.18

 

http://www.csd.toshiba.com/cgi-bin/tais/support/jsp/downloadDetail.jsp?soid=3373434&pf=true

 

 

If anyone tried it, let us know how it turns out.

========================================================
QOSMIO - x505 q8102X
i7-2630QM , GTX 460m , 18.4" screen @ 1680x945p
Member
Buddy23
Posts: 2
0

Re: Qosmio w NVIDIA 460M can run Dragon Age 2 at Max Settings!

I have the Qosmio X870 with nvidia drivers 296.18 and they work perfectly.

And I also tried the new ones 310.70 and they didn't work very well and I went back to the

296.18

Occasional Contributor
boidsonly
Posts: 10
0

Re: Qosmio w NVIDIA 460M can run Dragon Age 2 at Max Settings!

I installed the 310.70 nvidia drivers on my x505-q898 back in Dec.  It has been running fine since.  Prior versions did not fare so well and I had to revert to the OEM drivers.

  It is def worth trying them out to see how they do on the x505's.  Always perform a backup before trying them so you can revert quickly if needed.