NO SOUND ON HDMI!!!

Reply
Member
Posts: 2

NO SOUND ON HDMI!!!

I HAVE TOSHIBA SATELITE A505

IS ONLY 3 MONTHS SINCE I BOUGHT IT AND I HAD TO FORMAT IT ONCE ALREADY

SINCE I FORMAT IT I CAN USE HDMI CAUSE THE SOUND REMAINS ON THE LAPTOP.

ONLY VIDEO IS TRANSERED TO MY TV.

 

DOES ANYONE KNOW WHY?

IS IT CAUSE OF THE FORMAT?

OR DO I HAVE TO RESET SOME SETTINGS??

ANYWAY,IF ANYONE KNOWS IM OPEN TO SUGGESTIONS...

THANKS

Occasional Contributor
Posts: 24

Re: NO SOUND ON HDMI!!!

A little effort on your part would bring up some suggestions in the board search for e.g.

 

http://forums.toshiba.com/t5/Qosmio-Laptops/no-audio-from-hdmi-cable/m-p/9754#M366

Qosmio X505-880 Intel i7CPU Nvidia G360M Bios2.90
Member
Posts: 2

Re: NO SOUND ON HDMI!!!

thanks but i followed this:

Go to the lower right corner of the desktop, in the system tray.

 

Right click the Speaker Volume icon (RealTek High Definition Audio)

 

Choose Playback Devices

 

Double-Click on RealTek HDMI Output

 

Check that it's enabled, the level is 100%, etc.

 

 

Also make sure the volume isn't muted anywhere, it does play sound through the laptop speakers?

 

 

i cant find "RealTek HDMI Output" to click it....

whats wrong??

why sounds comes from my laptop and HDMI "sends" only video to my TV????

it wasnt like this before....

Super Advisor
Posts: 1,472

Re: NO SOUND ON HDMI!!!

Have you checked the settings under sound in control panel?

Welcome to the Toshiba user forums.
For those of you who do not know what a user forum is, it is a community of users who volunteer time to help other users. Anyone can participate. It's 100% voluntary.
Being super active is never a requirement
Member
Posts: 1

Re: NO SOUND ON HDMI!!!

Hey if you haven't already figured out how to fix the problem, we figured it out. We were having that same problem...but if you right click on the speakers just like the last forum said, then check the show disabled devices option. This should make the HDMI speakers show up. Hope this helps.