Can you remove the case of the Qosmio X500?

Reply
Member
Posts: 2
Accepted Solution

Can you remove the case of the Qosmio X500?

Hi,

 

Is it possible to remove the case of the Qosimo X500 without having to send it to Toshiba?

 

I have removed all the screws that I can see, but the top panel is still attached, there appears to be a screw underneath the plastic Smiley Frustrated

 

I post this in a hope that someone has done this before, and noticed something I didnt.

 

I have looked for guides but I couldnt find any, if I missed one please link me.

 

Regards,

 

Joe

 

 


Accepted Solutions
Regular Advisor
Posts: 294

Re: Can you remove the case of the Qosmio X500?

I wouldn't mess with it, unless you don't care about voiding the warranty.

 

There's a site out there with the dissasemble for the x500 (505).  Kind of afraid to post on here.  Goto http://forum.notebookreview.com/toshiba/ and there's a post there.

 

Good luck

 

 

========================================================
QOSMIO - x505 q8102X
i7-2630QM , GTX 460m , 18.4" screen @ 1680x945p

View solution in original post


All Replies
Regular Advisor
Posts: 294

Re: Can you remove the case of the Qosmio X500?

I wouldn't mess with it, unless you don't care about voiding the warranty.

 

There's a site out there with the dissasemble for the x500 (505).  Kind of afraid to post on here.  Goto http://forum.notebookreview.com/toshiba/ and there's a post there.

 

Good luck

 

 

========================================================
QOSMIO - x505 q8102X
i7-2630QM , GTX 460m , 18.4" screen @ 1680x945p
Member
Posts: 2

Re: Can you remove the case of the Qosmio X500?

Thanks alot Smiley Happy

Super Advisor
Posts: 1,472

Re: Can you remove the case of the Qosmio X500?

http://www.irisvista.com/tech/laptops/Toshiba-Satellite-A505/removing-optical-drive-1.htm

 

Make sure that you get it back together perfectly.  If Toshiba repair techs can tell that it has been opened then it is possible that it could void the warranty.   So if you are opening it to upgrade it, you could be causing yourself more trouble than the upgrade is worth at this time.

 

 

Welcome to the Toshiba user forums.
For those of you who do not know what a user forum is, it is a community of users who volunteer time to help other users. Anyone can participate. It's 100% voluntary.
Being super active is never a requirement
Occasional Contributor
Posts: 26

Re: Can you remove the case of the Qosmio X500?

[ Edited ]

Flagged as resolved but for others interested heres the full maintenence manual for the x500 seris: 

[ URL removed due to copyright violation ]

 

disassembly manual for the x300 series: http://www.irisvista.com/tech/laptops/Toshiba-Qosmio-X305/laptop-disassembly-1.htm

Qosmio x505-Q850 :Core i7 720QM 1.6GHZ 2x500GB 6GB
Apple MBP: Core i7 620M 2.66GHz 500GB 4GB
ASUS: Core i7 920 2.66GHz(4.06GHz) 6TB 12GB
HP nc6220: Centrino 2.13GHZ 320GB 2GB RAM
HP Pavilion a705w: Celeron 2.93 500GB 256MB RAM
HP Pavilion DV6000: No idea but it was crap!! 1.5GHz 80GB 512MB RAM