Reply
Member
talmarsh
Posts: 3
0
Accepted Solution

Z835 Models

Hello,


I searched all over and couldn't find the data.


What are the differences between the P330 and the P360 models?
And what's the difference between these (the "P3xx") and the ST6N and other "ST"s?

 

Thanks in advance!

Ace Advisor
Jerry_Lippey
Posts: 33,072

Re: Z835 Models

[ Edited ]

Links to the specs. I notice right off the P360 has Bluetooth.

 

Portege Z835-P330

 

Portege Z835-P360

 

You can look up the others the same way I did.

-Jerry
Member
talmarsh
Posts: 3
0

Re: Z835 Models

Great thanks! By changing the address I can get to the other models as well!

 

I still wonder if there's any change in build and exact models of internal components (such as FAN, SSD's specific models...).

Ace Advisor
Jerry_Lippey
Posts: 33,072
0

Re: Z835 Models


I still wonder if there's any change in build and exact models of internal components (such as FAN, SSD's specific models...).


I doubt it. To keep costs down, OEMs use as much of the same stuff as possible. Sometimes you'll discover vestiges that don't do anything.

-Jerry
Member
talmarsh
Posts: 3
0

Re: Z835 Models

One more thing I noticed - a mistake or difference in design? :smileyfrustrated:

 

P330:

"...Input Devices
 Premium Spill-resistant Raised Tile backlit Keyboard (black)
 Touch pad...

Physical Description
 Ultimate Silver..."

 

P360:

"...Input Devices 

• Premium Spill-resistant Raised Tile Keyboard (black)
o LED backlit
• Touch pad...

Physical Description
• Magnesium Alloy Casing in Silver
o Honeycomb Rib Structure Reinforcement..."

Ace Advisor
Jerry_Lippey
Posts: 33,072
0

Re: Z835 Models

My best guess is that it's just two different people writing the specs.

 

You can settle it easily by calling ToshibaDirect at 800-597-4512.

-Jerry
Regular Advisor
alexuw
Posts: 294
0

Re: Z835 Models

[ Edited ]

The P-subseries are the BestBuy models of the z835 [All the other z835/z830 do not include the BestBuy PC Software].  The P330 is the standard model with i3, backlit keyboard, and a 128 GB SSD.  The P360 is exactly the same with one exception: it has Bluetooth.  Basically the P330 is the older model that launched in November, the P360 is the newer refreash model that  Bestbuy carries.

 

BestBuy z835-P330

 

BestBuy z835-P360

 

 

========================================================
QOSMIO - x505 q8102X
i7-2630QM , GTX 460m , 18.4" screen @ 1680x945p