03-01-2012 10:04 AM
Hello,
I searched all over and couldn't find the data.
What are the differences between the P330 and the P360 models?
And what's the difference between these (the "P3xx") and the ST6N and other "ST"s?
Thanks in advance!
Solved! Go to Solution.
03-01-2012 01:31 PM - edited 03-01-2012 01:32 PM
Links to the specs. I notice right off the P360 has Bluetooth.
You can look up the others the same way I did.
03-02-2012 05:34 AM
Great thanks! By changing the address I can get to the other models as well!
I still wonder if there's any change in build and exact models of internal components (such as FAN, SSD's specific models...).
03-02-2012 06:09 AM
I still wonder if there's any change in build and exact models of internal components (such as FAN, SSD's specific models...).
I doubt it. To keep costs down, OEMs use as much of the same stuff as possible. Sometimes you'll discover vestiges that don't do anything.
03-02-2012 06:34 AM
One more thing I noticed - a mistake or difference in design? ![]()
P330:
"...Input Devices
Premium Spill-resistant Raised Tile backlit Keyboard (black)
Touch pad...
Physical Description
Ultimate Silver..."
P360:
"...Input Devices
• Premium Spill-resistant Raised Tile Keyboard (black)
o LED backlit
• Touch pad...
Physical Description
• Magnesium Alloy Casing in Silver
o Honeycomb Rib Structure Reinforcement..."
03-02-2012 06:39 AM
My best guess is that it's just two different people writing the specs.
You can settle it easily by calling ToshibaDirect at 800-597-4512.
03-02-2012 10:01 AM - edited 03-02-2012 10:06 AM
The P-subseries are the BestBuy models of the z835 [All the other z835/z830 do not include the BestBuy PC Software]. The P330 is the standard model with i3, backlit keyboard, and a 128 GB SSD. The P360 is exactly the same with one exception: it has Bluetooth. Basically the P330 is the older model that launched in November, the P360 is the newer refreash model that Bestbuy carries.
Copyright © 2013 Toshiba America Information Systems, Inc. All rights reserved.