07-21-2012 08:24 AM
I just got a R935-ST2N02 and wanted to use Bitlocker for the system drive. Is there a way to enable TPM or is this only available on certain R930's? The instructions are kinda cryptic and the utility installer just runs but doesn't appear to do anything. Any help from "the cloud" would be appreciated...
Solved! Go to Solution.
07-21-2012 03:30 PM
..is this only available on certain R930's?
You got it. TPM comes with the Toshiba EasyGuard stuff.
As you can see from the specs above, some have it and some don't.
07-21-2012 03:47 PM
Jerry:
Thanks much for clearing that up...
Mark
07-21-2012 03:55 PM
Happy to help, Mark.
Copyright © 2013 Toshiba America Information Systems, Inc. All rights reserved.