Portege R705

Reply
Member
Posts: 1

Portege R705

Each time I start up my laptop windows execute some kind of assessment over the files to see if there is not coherence problems.

In the past it did not execute that and is very annoying to wait this long process.

As a matter of fact if you watch from the beginning you can cancel the process.

pls help me

Posts: 47,473
Topics: 83
Kudos: 8,999
Solutions: 3,196
Registered: ‎12-04-2008

Re: Portege R705

Maybe if you would explain things so we can understand, we could help.

 

Start by telling us which Portege R705 you have. What is the part number? Which country? Which Windows? And so forth..

 

Then describe in terms we can understand what it is you are looking at. We cannot see it. Please quote precise fragments from what you see on your screen. Don't paraphrase. Spelling counts.

 

There is lots of space here. Don't be afraid to use it.

-Jerry
Channel 9