09-07-2012 04:01 PM - edited 11-09-2012 05:38 AM
I can't seem to find drivers for the following two:
PCI Simple Communication Controller
Toshiba F3507g Broadband Mobile Device
I also have an unknown device.
Also I two features that don't work anymore: Bluetooth and FingerPrint. I can live without the FingerPrint, but I need my Bluetooth for work.
Using Windows 8 x64
[Later edit]
Got working:
Still no solution for the HDD protection utlity, yet.
09-08-2012 08:34 AM
Victor, this is the site for U.S. machines. Yours is a European model. You can find drivers, support and a Forum for your machine HERE.
C.B.
09-14-2012 08:23 AM
Sorry didn't notice it. But anyway, I know about that website. The only problem is that it has no drivers for windows 8. Only for 7. And even if some do work on win8, not all of them do. Like the FingerPrint Utility.
09-14-2012 08:31 AM - edited 09-14-2012 08:32 AM
Which M750 do you have?
The model looks something like Portégé M750-112 and the part number like PPM75E-02000JG3.
11-07-2012 01:23 PM - edited 11-07-2012 01:25 PM
it's M750-10G
Part number: PPM75E-00S00JG3
Sorry for the late reply.
[edit] I did manage to install a Finger Print software (was easier than I thought), but I'm still missing a lot of devices I had on 7 and XP. I can live withouth most of them, I can live with no 3G utility, but one thing that annoys me the most is that I can't set up my screen buttons. I have a small joystick and 4 buttons and none of them do what they are suppose to do.
11-07-2012 01:42 PM
Portégé M750-10G (PPM75E-00S00JG3)
Downloads are here.
Unfortunately, Toshiba does not support that model for upgrade to Windows 8. So you're on your own. Good luck!
Windows 8 Upgrade - Supported Models
11-09-2012 01:28 AM - edited 11-09-2012 01:31 AM
Well thanks anyway.
If anyone else has the same problems as me here's what I managed to get working again:
Also if you want the radar thingy just install Config Free (Toshiba Europe)
Still no solution for:
All the drivers up there are in stalled on Windows 8 x64. From what I saw there are more drivers (from Windows 7) for the x82 (32bit) version. I will install the 32bit version this weekend and see if I can get more things working on it. I'll update my first post when that is done.
[L.E] forgot to add a link: Toshiba Portege Europe Forum
11-09-2012 06:19 AM
You might learn more in the proper forum. You'll also find folks who appreciate what you've learned.
Toshiba Support Forums in Europe
Copyright © 2013 Toshiba America Information Systems, Inc. All rights reserved.